TI Home > News Releases

News Releases

TI Delivers Industry's First Location Detection System-on-Chip for ZigBee® Wireless Sensor Networking

Highly Integrated Device Accurately Calculates Location in Mesh Networks

Jun 11, 2007

DALLAS (June 11, 2007) - Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced the industry's first System-on-Chip (SoC) solution with a hardware location engine targeting low-power ZigBee&#174/IEEE 802.15.4 wireless sensor networking applications. The CC2431, from the company's Chipcon product line, targets applications such as asset and equipment tracking, inventory control, patient monitoring, remote controls, security and commissioning networks. The device is supported by TI's Z-StackTM protocol stack. (See www.ti.com/cc2431-pr.) 

The CC2431 is based on the industry's first available SoC solution for low-power RF applications, the CC2430. Both devices combine the excellent performance of the industry-leading CC2420 RF transceiver core with an enhanced 8051 microcontroller, up to 128 kB flash memory, 8 kB of RAM and many additional features - all in a small 7mm x 7mm package.

The CC2431's RSSI-based location engine accurately calculates the node's position based on the receive signal strength from CC2430-based reference nodes with known locations and can then send the location information to a collector (e.g. computer, PDA, handset). This capability reduces network traffic and communication delays compared to centralized location systems. In typical applications, accuracy of 3-5 meters can be achieved.

"Combined with the Z-Stack, the CC2431 provides the market's most competitive ZigBee solution and illustrates the innovation and market leadership of the Chipcon product line," said Art George, senior vice president of TI's high-performance analog business. "Customers will now be able to develop reliable and robust wireless networks, while reducing time-to-market and minimizing production costs."

TI's Z-Stack protocol software is designed to the ZigBee 2006 specification and supports multiple platforms, including the CC2431, CC2430 and CC2420+MSP430 platform. The Z-Stack has been awarded the ZigBee Alliance's golden unit status by the ZigBee test house TUV Rheinland and is used by thousands of ZigBee developers worldwide. The Z-Stack is available for free downloading at www.ti.com/zigbee.

Availability and Packaging

The CC2431 is sampling now, with volume production scheduled for 3Q 2007. The device is available in a RoHS-compliant 7mm x 7mm QLP-48 package and is priced at $6.45 in 1,000-piece quantities (suggested resale pricing). The CC2430 is in volume production and available from TI and its authorized distributors. Start your development today with the comprehensive ZigBee development kit, CC2431ZDK.

Low-Power RF Developer Network

TI's Low-Power RF Developer Network enables customers to find a suitable partner to assist with hardware design, modules, embedded software, gateways, commissioning tools, etc. The Low-Power RF Developer Network consists of recommended companies, RF consultants, and independent design houses that provide a series of hardware module products and design services (www.ti.com/lprfnetwork).

ZigBee: Wireless Control That Simply Works

Texas Instruments is proud to be a Promoter level member of the ZigBee Alliance. The Alliance is an association of companies working together to enable reliable, cost effective, low-power, wirelessly networked, monitoring and control products based on an open global standard. The ZigBee Alliance membership comprises technology providers and original equipment manufacturers worldwide. Membership is open to all. Additional information can be found at www.zigbee.org.