TI Home > News Releases

News Releases

TI Unveils Battery Management Chips to Manage and Protect Multi-Cell, Li-Ion Battery Packs

Impedance Track(TM) Gas Gauge Chipset Taps Unused Energy, Provides Safety and Security Features

Dec 18, 2006

DALLAS (Dec. 18, 2006) -- Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced several new battery management integrated circuits (ICs), including its next-generation Impedance TrackTM  "gas gauge" chipset, to improve battery performance and protect multi-cell, lithium-based battery packs used in notebooks and other systems.  

Next-Generation Impedance Track Gas Gauge

TI's bq20z90 next-generation Impedance Track battery gas gauge chipset, which integrates new state-of-the-art battery authentication technology, is designed to work with TI's newest analog front end (AFE) protection IC. Requiring a third fewer components than its predecessor, the 99-percent accurate bq20z90 chipset was designed with ease-of-use and smallest real estate in mind. The gas gauge closely monitors battery capacity, impedance, cell balance, open-circuit voltage and other critical parameters of a 7.2-V, 10.8-V or 14.4-V battery pack and reports the information to the system host controller over a serial-communication bus. See: www.ti.com/sc06160


TI's Impedance Track gas gauge technology, launched in 2004 with the

bq20z80

chipset, precisely measures changes in impedance, or resistance caused by battery age, temperature and cycle life, to accurately predict run-time of battery packs with two, three and four cells in series. An exact "starting position" is determined for instant state-of-charge, and total capacity is calculated from the amount of capacity that exists, which eliminates the need for a full-charge and discharge cycle.


The

bq20z90

drives a three-, four- or five-segment LED display for remaining capacity indication. For those designs that do not require the display indicator, TI also introduced its

bq20z70

gas gauge chipset without the LED display driver.


Front-End Battery Protection

The bq20z90 is designed to work with TI's new bq29330 AFE protection circuit with two integrated linear dropout regulators (LDOs) to further maximize functionality and reduce external component count. The device utilizes an I2C communications interface to allow the bq20z90 to monitor safety battery conditions such as voltage, individual cell voltages and cell-balancing data, and report the information to the host system. See: www.ti.com/sc06160b


A designer can program critical safety parameters such as current protection thresholds and delays into the

bq29330

to increase flexibility of the battery management system. The device also provides protection for overload short-circuit in charge and discharge conditions, while providing battery cell over-voltage and under-voltage protection.


Integrated SHA-1 Based Authentication

The bq20z90 integrates SHA-1, 128-bit decryption functionality, which easily identifies potentially unsafe batteries not approved by original equipment manufacturers for use in their devices. If the battery information checks out, the system can allow normal system operation with the battery pack. A manufacturer can program the system to take action to protect the consumer if the battery pack response is not correct, or if the battery pack is not approved or determined to be defective. In addition, TI introduced a bq26100 protection device for those designers who prefer a discrete implementation of the SHA-1 protection feature. See: www.ti.com/sc06160c


Smart Battery Test Board

In addition to the new battery gas gauge chipset, TI has developed a unique development platform aimed at battery pack suppliers. TI's new bqMTester smart battery development board simplifies production of battery modules at a fraction of the cost. bqMTester eliminates the need for an onboard computer and expensive calibration/traceable power supplies and electronic loads. It calibrates and programs electronic smart battery modules based on advanced battery fuel gauges, such as the bq20z90, bq20z80 and bq20z70 devices with Impedance Track. In addition, bqMTester makes tracking battery modules in production easier by programming serial number, date, pack lot code and other defaults. The bqMTester board can be ordered at www.ti.com/bqmtester


Pricing and Availability

The bq20z90 and bq20z70 gas gauge chipsets, bq29330 protection AFE and bq26100 authentication circuit are available in volume production from TI and its authorized distributors. The bq20z90 is packaged in a 30-pin thin shrink small outline package (TSSOP), the smaller bq29z70 in a 20-pin TSSOP, the bq29330 in a 30-pin TSSOP package and the bq26100 in a tiny, 6-pin SON package. Suggested resale pricing in 1,000 piece quantities is $3.30 for the bq20z90, $2.90 for the bq20z70, $1.45 for the bq29330, and $1.30 for the bq26100


Evaluation modules for the

bq20z90

gas gauge chipset, the bqMTester development board, reference designs, application notes and technical documentation are available through 

www.ti.com/impedancetrack