TI Home > News Releases

News Releases

Basestation manufacturers can meet carrier requirements to support data-intensive, next-generation mobile applications while keeping an eye on costs with TI's new powerful, scalable LTE platform

TI's 1.2 GHz DSP and optimized software library allows OEMs to extend current platforms quickly and easily

Feb 9, 2009

DALLAS (Feb. 9, 2009) - Addressing the MIPS-intensive LTE (Long Term Evolution) wireless standard, Texas Instruments Incorporated (TI) [NYSE:TXN] has developed the 1.2GHz TMS320TCI6487, a three core digital signal processor running at 3.6GHz coupled with a powerful software library that delivers all of the performance necessary to support LTE's complex algorithms. With TI's new LTE solution, OEMs can extend their current basestation platforms to include new features and more complex algorithms without designing a new board. In addition, TI's optimized software library for LTE leverages specialized accelerators and instructions that further improve the efficiency of today's systems. For more information, go to www.ti.com/morelte.

"More than 18 carriers around the world have recently announced plans to deploy LTE to the cumulative tune of $8.5 billion by 2012 for wireless infrastructure equipment," said Jagdish Rebello, director and principal analyst of consumer and wireless research, iSuppli. "A key driver for LTE deployment is the consumer's insatiable demand for data-intensive applications running on mobile internet devices or smartphones, including interactive remote games, streaming video and location-based applications, which require significantly more bandwidth and no tolerance for latency. To meet these challenging network requirements while keeping an eye on costs, basestation OEMs and carriers need a powerful, scaleable solution similar to the one TI is providing."

"Proof that TI delivers parts with our customer's architecture in mind and provides the most efficient path to deployment, our 1GHz TCI6487 is currently used in eight of the top ten LTE OEM systems going through development, lab, and field trials today," said Kathy Brown, general manager of TI's wireless basestation infrastructure group. "By increasing the performance of our C64x+™-based digital signal processor (DSP), we enable our customers to support new features and requirements quickly and effectively, reducing cost and accelerating time to market."

To achieve a successful LTE deployment, robust software is a requirement. TI's third generation LTE software library release includes optimized functions for all necessary signal processing elements. In addition, TI has released software to use on-chip acceleration to support decoding the uplink channel quality information (CQI), thereby saving up to 1 GHz of DSP processing - a savings equivalent to adding an additional core to the DSP. A complete physical layer reference design incorporating TI's LTE library is available from Tata Elxsi and mimoOn.

TI also offers a reference platform from Commagility, enabling customers to quickly evaluate their networks and optimize system design, speeding LTE deployments. In addition to the reference platform, TI provides the complete analog signal chain for LTE, including data converters, RF products, power management, clocks and amplifiers.

Features and benefits

The TCI6487 contains three DSP cores, each running at 1.2 GHz. Each core has its own dedicated 1 Mbyte of L2 with 32k of L1 data and program cache minimizing off-chip memory access and enabling efficient software architectures. TI's easy-to-use and efficient compiler tools reduce the time required to develop and test new software features.

The TCI6487 includes additional high performance accelerators and peripheral interfaces, which are optimized for cellular infrastructure products. Each DSP core contains one RSA unit that can accelerate the decoding of LTE CQI information - a savings of up to 1 GHz per sector for 20 MHz LTE systems. The flexibility and ease of use of TI DSPs makes this product ideal for multi-standard designs or as the core technology for multiple, targeted designs.

In addition to LTE software libraries, TI provides optimized libraries for WiMAX and WCDMA to further enable multi-standard developments. These libraries enable higher channel density as well as lower power per channel. Developed and tested within TI's carrier-class environment, the inclusion of this software allows basestation OEMs to better focus on their system level solutions.

Availability

The 1.2 GHz TCI6487 will be sampling in 1Q09 to targeted cellular infrastructure customers and will be available to the broader market in 2Q09. It will be on display at the Mobile World Congress Conference in Barcelona, February 16-19, Hall 8, TI's booth #8A84.