TI Home > News Releases

News Releases

National Semiconductor Expands PLL Product Line with the Addition of Two PLLatinum PLLs for Base Stations

Low Phase Noise, High Performance Make LMX2346 and LMX2347 Single Frequency Synthesizers Ideal for Wireless Infrastructure Applications

Aug 12, 2002

August 12, 2002?National Semiconductor Corporation (NYSE:NSM) today announced the addition of two new frequency synthesizers to its PLLatinum? line of phase locked loops (PLLs) for wireless infrastructure applications.  LMX2346 and LMX2347 are National?s next generation of fixed radio PLLs and are pin- and software-compatible with current LMX2323 PLLs, providing easy upgrade.  The LMX2346 and LMX2347 feature very low phase noise for increased radio sensitivity, allowing fewer dropped calls, extended base station range and improved voice quality.  In addition, low power performance and small chip scale packaging make the PLLs ideal for use in 2, 2.5, 3G and future mobile telephone infrastructure equipment including base stations, WLANs and other wireless communications systems. 

?With the LMX2346 and LMX2347, system designers can better maximize the performance of wireless applications.  These PLLs are designed to operate in space constrained designs, while minimizing noise for improved radio sensitivity,? said Michael Sanders, product marketing manager for National?s wireless division. ?As system designers pack more functionality and equipment into existing space, product designs like the LMX2346 and LMX2347 ? that combine high performance low noise capability with a small footprint ? are increasingly important to the overall performance of the end product.?

About the LMX2346 and LMX2347
LMX2346 and LMX2347 are high performance frequency synthesizers that offer all the features of National's PLLatinum product line.  The LMX2346 and LMX2347 are manufactured using National's advanced BiCMOS process.  Employing a proprietary digital phase locked loop technique, the PLLs generate very stable, low noise control signals for UHF and VHF voltage controlled oscillators (VCOs).

Both PLLs feature low phase noise of -91dBc/Hz at 900MHz and -85dBc/Hz at 1960MHz, which enables better radio sensitivity.  Other features that help system designers improve phase noise performance are a charge pump power supply voltage of up to 6V, allowing the use of low gain VCOs; a selectable oscillator input buffer mode that minimizes buffer noise current; and the support of higher reference frequencies up to 104MHz.

In addition, the LMX2346 and LMX2347 operate at frequencies up to 2.0GHz and 2.5GHz, respectively, and offer 2.7V to 5.5V operation, low current consumption of 6.5mA and digital lock detect.

Pricing and Availability
The LMX2346 and LMX2347 are available in both CSP-16 and TSSOP-16 packages and priced starting at $2.05 and $2.50, respectively.  All prices are in 1000-unit quantities.  For more information on these products, visit National's web site at http://www.national.com/pf/LM/LMX2346.html
and http://www.national.com/pf/LM/LMX2347.html.  To view a high-resolution downloadable photo, visit National's photo gallery at http://www.national.com/company/pressroom/gallery/wireless.html.

LMX2346 and LMX2347 are featured in National's WEBENCH? - EasyPLL interactive simulation tools, the online design environment that enables engineers to design and simulate PLL and loop filter circuit designs.  Visit National's WEBENCH at: http://wireless.national.com.

About National Semiconductor
National Semiconductor is the premier analog company driving the information age. Combining real-world analog and state-of-the-art digital technology, the company is focused on the fast growing markets for wireless handsets; displays; information infrastructure, and information appliances. With headquarters in Santa Clara, California, National reported sales of $1.5 billion for its most recent fiscal year and has about 10,000 employees worldwide. Additional company and product information is available on the World Wide Web at www.national.com
.