Dec 9, 2003
![]() |
Bluetooth Americas Conference, San Jose, CA - December 9, 2003 - National Semiconductor Corporation (NYSE:NSM) today announced its newest Bluetooth® product family that complies with the recently ratified Bluetooth Specification Version 1.2.
The LMX5252 is a Bluetooth radio transceiver that delivers the highest level of RF integration available today. The LMX5452 combines the radio with an enhanced Bluetooth 1.2 baseband processor into a small micro-module package. Both products offer a high level of analog and RF integration in a small footprint, saving space and cost while enhancing performance.
"National's LMX5452 micro-module packaging technology, combined with the increased level of radio integration, makes this new Bluetooth product family a superior solution for mobile phone and computing applications," said Malcolm Humphrey, director of National's Device Connectivity Division. "What customers care about is the size of the solution and ease of design. Using National's micro-module solution reduces RF board complexity, enabling mobile device manufacturers to integrate the device directly onto their main board design, and reducing the need for a traditional and more expensive module approach."
Bluetooth wireless technology enables users to exchange information between a wide variety of computing and communications systems, including mobile phones, PCs, printers, PDAs, and even your automobile, without connecting wires or cables. The new features found in Bluetooth Specification Version 1.2 include faster connecting times, improved voice transmissions and adaptive frequency hopping (AFH) for improved coexistence of Bluetooth with other 2.4GHz devices.
About the LMX5252
The LMX5252, in a 36-pin LLP package measuring 6mm by 6mm by 0.8mm, is a highly integrated .18 micron CMOS Bluetooth radio transceiver with an integrated Tx/Rx switch and baluns. It supports multiple system clock frequencies of 10 to 40MHz, and has a typical Rx sensitivity of -84dBm. The LMX5252 is ideal for applications where Bluetooth baseband functionality is already integrated into the primary processor, including systems using National's CP3000 connectivity processors.About the LMX5452
The LMX5452, in a 60-pin micro-module BGA package measuring 9mm by 6mm by 1.2mm, combines the Bluetooth transceiver with a baseband processor. The baseband processor features full Bluetooth 1.2 functionality and firmware, and an enhanced HCI command structure. In addition, it combines on-chip, ROM-based memory with a seamless memory patch controller and flexible patch RAM.Pricing and Availability
Samples of the LMX5252 are available now. Production quantities will be available later this month. In high volumes, the LMX5252 is priced below $3. Samples of the LMX5452 are available to select customers now with production quantities available in the first quarter of 2004. In high volumes, the LMX5452 is priced below $4. More information on the products is available at wireless.national.com. For more information on National's wireless products, visit http://wireless.national.com. To view a high-resolution downloadable photo of the LMX5452, visit National's photo gallery at http://www.national.com/company/pressroom/gallery/wireless.html.National at Bluetooth Americas 2003 Conference
National Semiconductor will demonstrate the LMX5252 and LMX5452 at the Bluetooth Americas Conference in San Jose, December 9-11, in National's booth number #505. The company will also present "Automotive: The Driving Application for Bluetooth" on December 9 at 2:30 p.m. by Abdul Aleaf, senior applications manager for National Semiconductor. More information on National's activities at the Bluetooth Americas Conference may be found at http://www.national.com/events/.About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high performance analog devices and subsystems. National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, imaging sensors and data conversion solutions. National's key markets include wireless handsets, displays, PCs, networks and a broad range of portable applications. With headquarters in Santa Clara, California, National reported sales of $1.67 billion for fiscal 2003, which ended May 25, 2003. Additional company and product information is available at www.national.com.