TI Home > News Releases

News Releases

National Semiconductor Introduces High-Precision Amplifier Line for Improved Accuracy in Industrial, Medical and Automotive Applications

Oct 5, 2004

October 5, 2004 - National Semiconductor Corporation (NYSE:NSM) today introduced a new family of high-precision, high-performance amplifiers to herald its entry into the burgeoning precision market.  National’s linear monolithic precision (LMP™) line addresses existing precision applications and positions National to provide next-generation products for a market that is increasingly focused on accuracy.  The first parts in the new LMP family are the LMP2011, LMP2012 and LMP2014, for broad-based applications in industrial, medical and automotive electronics.

 The LMP2011/12/14 are single, dual and quad high-precision amplifiers with a very low offset voltage of 25 microvolts and wide bandwidth of 3 MHz for accurate signal amplification and reduced error for applications where DC precision and strong AC specifications are needed.

“National Semiconductor is very excited to introduce the new LMP line and announce a new thrust area for the company,” said Erroll Dietz, vice president of National’s Amplifier product group.  “Our goal is to provide customers with the highest-accuracy parts on the market, and we’re on track to do just that.  Our high-performance family of analog amplifiers not only provides very high precision over time and temperature, but also an extended temperature range.  Thanks to National’s long history of innovation in analog design, we’re in a great position to support a broad range of demanding precision applications.”

Stellar Specifications
National’s LMP2011/12/14, in addition to having very low input offset voltage (Vos), are very stable over time and temperature (0.015 microvolts/degrees Celsius).  These parts feature a high common mode rejection ratio, power supply rejection ratio, and high open loop gain, all in excess of 120dB.  The LMP2011/12/14 also provide flat band noise of 35 nanovolts per root hertz with no 1/f noise.

Pricing and Availability
National’s LMP2011 is available now in SOT23-5 packaging and is priced at $0.98, the LMP2012 is available now in MSOP-8 packaging and is priced at $1.40, and the LMP2014 is available now in TSSOP-14 packaging and is priced at $2.75 in 1,000-unit quantities.  For more information on National’s LMP2011/12/14, visit http://www.national.com/pf/LM/LMP2011.html
, http://www.national.com/pf/LM/LMP2012.html and http://www.national.com/pf/LM/LMP2014MT.html.    For more information on National’s amplifier products, visit http://amplifiers.national.com.  A large selection of amplifiers is supported by National’s Amplifiers Made SimpleSM WEBENCH® online design tool.  To explore these solutions visit http://webench.national.com.  To learn more about designing with amplifiers, visit National’s library of online seminars.  To view a high-resolution downloadable photo of these products, visit National's photo gallery

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high performance analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National's key markets include wireless handsets, displays, PCs and laptops.  The company's analog products are also optimized for numerous applications in a variety of electronics markets, including medical, automotive, industrial, and test and measurement.  Headquartered in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004.  Additional company and product information is available at www.national.com.