TI Home > News Releases

News Releases

National Semiconductor Introduces High-Speed Video Multiplexers

Newest LMH Video Multiplexing Amplifiers Achieve Highest Bandwidths and Fastest Switching Times in the Industry

Nov 9, 2004

ELECTRONICA, Munich—November 9, 2004—National Semiconductor Corporation (NYSE:NSM) today launched the LMH6574, the industry’s fastest single 4:1 video multiplexing (MUX) amplifier, and the LMH6572, the fastest dual-supply, triple 2:1 RGB (red, green, blue) MUX amplifier on the market.  By leveraging its VIP10 process technology, National has achieved higher bandwidth and slew rates, faster switching times and lower crosstalk than any competitor.  These features enable higher video resolutions with less video distortion for professional video, security systems, HDTV, NTSC and PAL video systems, analog video routers and switchers, and other video applications.

"National is leading the industry with its high-speed video amplifiers,” said Erroll Dietz, vice president of National’s Amplifier product group.  “With the introduction of the LMH6574 and LMH6572, National is able to reduce crosstalk and decrease shadowing effects in the end application, delivering the highest level video and picture quality for our customers.”

High Speed, High Quality, High Performance
National’s LMH6574 is a single, high-speed, buffered 4:1 video MUX amplifier.  It achieves 400 MHz-3dB bandwidth (2Vpp) and 150 MHz 0.1 dB gain flatness to support switching of high video resolutions.  It features 8 ns switching time for faster switching between input signals.  It also provides 85 dB of channel-to-channel isolation for reduced interference from other channels.  Benefits include a clearer picture and less shadowing effects and artifacts.

National’s LMH6572 is a high-speed, buffered triple 2:1 RGB MUX amplifier.  It achieves 300 MHz-3dB bandwidth (2 Vpp) and 60 MHz 0.1 dB gain flatness, which supports RGB switching of higher video resolutions than the competition, both for existing and future video line rates, including UXGA.  The LMH6572 also features 10 ns switching time for faster switching between input signals.  It also provides 90 dB channel-to-channel isolation.

VIP10 Process
National's LMH6574 and LMH6572 are National’s newest amplifiers created using the VIP10 process.  Developed in National's wafer fabrication site in Arlington, Texas, the VIP10 process is a high-speed, dielectrically isolated, complementary BiCMOS process that utilizes deep trench technology on a bonded wafer for complete dielectric isolation and optimal high-speed amplifier performance.  The VIP10 process technology allows National to design the most power-efficient, performance-oriented high-speed amplifiers on the market today.

National’s LMH6574 and LMH6572 MUX amplifiers will be shown in National’s booth #506 in Hall A4 at the Electronica trade show in Munich, Germany, from November 9-12.

Pricing and Availability
National’s LMH6574 is available now in SOIC-14 packaging and is priced at $2.49, and the LMH6572 is available now in SSOP-16 packaging and is priced at $3.50, both in 1,000-unit quantities.  For more information on National’s LMH6574 and LMH6572 visit http://www.national.com/pf/LM/LMH6574.html
and http://www.national.com/pf/LM/LMH6572.html.  For more information on National’s amplifier products, visit http://amplifiers.national.com.  A large selection of high-speed amplifiers is supported by National’s Amplifiers Made SimpleSM online design tool.  To explore these solutions visit http://webench.national.com.  To learn more about designing with amplifiers, visit our library of online seminars.  To view a high-resolution downloadable photo of these products, visit National's photo gallery

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high performance analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National's key markets include wireless handsets, displays, PCs and laptops.  The company's analog products are also optimized for numerous applications in a variety of electronics markets, including medical, automotive, industrial, and test and measurement.  Headquartered in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004.  Additional company and product information is available at www.national.com
.