TI Home > News Releases

News Releases

National Semiconductor Announces New High-Performance Converters that Slash Power Consumption in Cell Phones Up to 80 Percent and Extend Talk Time As Much as 90 Minutes

National’s New LM3200 is the First in a Revolutionary Family of Analog DC-DC Converters Optimized to Save Power and Reduce Board Space in Smart Phones, Wireless LANs, PDAs and other Portable Wireless Devices

Nov 9, 2004

SANTA CLARA, CA AND MUNICH, GERMANY—November 9, 2004—National Semiconductor Corporation (NYSE:NSM) today announced a new family of DC-DC converters optimized for powering radio frequency (RF) power amplifiers from a single lithium-ion battery. These new chips from National will enable cell phone makers to reduce power consumption by up to 80 percent, while increasing talk time as much as 90 minutes. The first cell phones to use National’s new LM3200 DC-DC converters will appear in the market by year-end.

With 2.5G and 3G wireless handsets gaining popularity, cell phones are becoming a one-stop multimedia station with features such as text messaging, email and software downloads. These new handsets require higher transmit-and-receive rates for (RF) power amplifiers, which mean that they consume more power. Because the RF power amplifier consumes 40 to 60 percent of the overall power budget, reduction of its power consumption will provide a significant increase in the battery life of a handset.

National’s new LM3200 is designed specifically to power RF power amplifiers. Compared with previous step-down switchers, the LM3200 has a high switching frequency that allows it to use small external components such as a 2.2 µH inductor. The LM3200 also has an analog voltage-control input that dynamically controls the output voltage of the device depending on the power requirements of the power amplifier. Its bypass operation allows it to support the power amplifier’s power requirement during peak usage periods to keep the phone running longer. The converter steps down an input voltage from 2.7V to 5.5V to a variable output voltage from 0.8V to 3.6V, while output voltage is set using a voltage-control analog input for adjusting power levels and efficiency of the RF power amplifier.

“With these new products, National is targeting the power amplifier—a previously unregulated  portion of the cell phone—to enable dramatic improvements in battery life and talk time,” said Peter Henry, vice president of National Semiconductor’s Portable Power Products Group. “National’s LM3200 features a small-size chip-scale package, high switching frequencies and compatibity with a wide variety of industry-standard platform reference designs that will enable our customers to offer phones and other portable devices with outstanding performance.”

Key Technical Specifications of National’s New LM3200
The LM3200 offers four modes for mobile phones and similar RF PA applications. Fixed-frequency pulse-width modulator (PWM) mode minimizes RF interference and provides efficient performance under typical operating conditions. Forced bypass mode turns on an internal bypass switch to power the PA directly from the battery. Automatic bypass mode minimizes dropout by turning on the bypass switch when the battery decays close to the output voltage. Shutdown mode turns the device off and reduces battery consumption to 0.1uA (typ.). The LM3200 is designed on National’s CMOS7 process, built at National’s plant in South Portland, Maine, and tested and assembled at the company’s facility in Melaka, Malaysia.

National’s LM3200 is available in a 10-pin lead-free micro SMD that measures only 2.2 mm by 1.8mm. A high switching frequency (2MHz) allows use of tiny surface-mount components. Only three external components, a 2.2uH inductor and two 10uF ceramic capacitors, are needed to complete the application circuit. National’s LM3200 is priced at $1.60 each in quantities of 1,000 pieces.

Note to editors: To view high-resolution downloadable photos, please visit: http://www.national.com/company/pressroom/gallery/power.html

About National’s Power Management Products
National Semiconductor is the number one supplier of power management ICs with 12.8 percent market share, according to iSuppli’s 2004 voltage regulator/reference survey.  National’s power management revenue grew 29.7 percent in 2003 over the previous year, compared to 17.3 percent growth for the industry during the same time period.  National's innovative power management products include best-in-class linear regulators; power monitoring, control and reference ICs; and switching converters, such as high-voltage ICs for DC/DC conversion, switched capacitor converters, lighting management ICs and inductive switching converters.  National's WEBENCH® online design tool allows designers to select a power management product, create and analyze a design, and then build custom prototypes that can be delivered within 24 hours.  More information about National’s power management products is available at
http://power.national.com.

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high performance analog devices and subsystems. National’s leading-edge products include power management circuits, display drivers, audio and operational amplifiers, and data conversion solutions. National's key markets include wireless handsets, displays, PCs, networks and a broad range of portable applications. With headquarters in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004. Additional company and product information is available at www.national.com
.