TI Home > News Releases

News Releases

National Semiconductor Technology Revolutionizes Temperature Sensing for Sub-Micron CPUs, ASICs and FPGAs

New Sensor Measures Temperature With Pinpoint Accuracy

National to Discuss Technology and Products at Intel Developer’s Forum

Feb 28, 2005

February 28, 2005 – In a breakthrough for thermal management accuracy, National Semiconductor Corporation (NYSE:NSM) today announced TruTherm™ thermal management technology, which uses a new measuring technique to provide pinpoint-accurate temperature measurement for chips with integrated thermal diodes. 

“Measuring the internal temperature of sub-micron CPUs and FPGAs with traditional methods generates results that are inaccurate and unpredictable,” said Suneil Parulekar, National Semiconductor’s senior vice president of the Analog Products Group. “To solve this problem, National’s new TruTherm technology relies on a new measuring technique to achieve an unmatched level of temperature reading accuracy.”

As computing systems and consumer electronics incorporate more sub-micron processors and FPGAs that tend to run hot, engineers need to design cooling fans into their systems to prevent overheating. By providing a pinpoint-accurate temperature reading, National’s TruTherm™ technology enables designers to achieve higher levels of performance, extend system life and reduce acoustic noise in systems using central processing units, graphics processors, field-programmable gate arrays and other integrated circuits developed in 90-nanometer and below processes. 

"More accurate temperature readings allow designers to optimize system performance, protect the system processor and lower acoustic noise," said Benson Inkley, senior processor applications engineer of Intel Corporation. "To support TruTherm technology, Intel will include additional parameters in the datasheet for our new 90-nanometer Pentium 4 processors."

New LM95231 Sensor with TruTherm Technology
National is producing a family of new temperature sensors featuring TruTherm technology. The first member of this family, the LM95231, is a high-precision, dual remote-diode temperature sensor with plus or minus 0.75 degrees Celsius accuracy. It features a precision sigma-delta analog-to-digital converter for reduced sensitivity to noise and includes digital filtering, remote-diode fault detection and local temperature sensing. The LM95231 is compatible with the SMBus 2.0 and I2C bus specifications.

The LM95231 is designed on National’s proprietary, analog-optimized advanced CMOS process, manufactured at National’s wafer fabrication plant in South Portland, Maine, and tested and assembled at the company’s facility in Melaka, Malaysia. 

National Presents at IDF
National Semiconductor's experts in thermal management design will introduce the TruTherm technology in a tutorial session at the Intel Developer’s Forum in San Francisco. The session, “Improve Acoustic Performance Using a New Processor Temperature Sensing Technique,” will be held from 3:30 p.m. to 4:20 p.m. on Thursday, March 3 at the Moscone Center.

Pricing and Availability
Limited samples of the LM95231 temperature sensor, packaged in an 8-pin MSOP, are available now. Production quantities will be available in May 2005 and priced at $1.50 in 1,000-unit quantities. For more information on National’s thermal management products, visit
http://www.national.com/appinfo/tempsensors/.
 
Note to editors:  To view a high-resolution downloadable photo of this product, visit National's photo gallery at
http://www.national.com/company/pressroom/gallery/temp.html.

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high-performance analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National's key markets include wireless handsets, displays, PCs and laptops.  The company's analog products are also optimized for numerous applications in a variety of electronics markets, including medical, automotive, industrial, and test and measurement.  Headquartered in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004.  Additional company and product information is available at
www.national.com.