TI Home > News Releases

News Releases

National Semiconductor Introduces Boomer Stereo Audio Power Amplifier For Flat-Panel Displays and Computer Sound Cards

May 18, 2005

May 18, 2005 - National Semiconductor Corporation (NYSE:NSM) today introduced the Boomer® LM4952 dual audio power amplifier primarily designed for high-power and space-constrained applications in flat-panel monitors, flat-panel televisions and computer sound cards. Boomer audio power amplifiers provide high-quality output power with a minimal number of external components.

The LM4952 is a stereo audio power amplifier with DC volume control. Eliminating external feedback resistors, an internal, DC-controlled volume control allows easy and variable gain adjustment. The audio amplifier is capable of delivering a 3.1W per channel to a four-Ohm, single-ended load with less than 1 percent total harmonic distortion plus noise (THD+N) when powered by a 12V DC power supply.

Requiring no bootstrap capacitors or snubber circuits, the LM4952 features a low-power- consumption active-low shutdown mode and an internal thermal shutdown protection mechanism along with short-circuit protection. Its advanced pop and click circuitry eliminates noises that would otherwise occur during turn-on and turn-off transitions.

Additional Features of the LM4952

  • Low quiescent current (18 mA typical)      
  • Stereo 3.8W output of RL = 4      
  • Power output (POUT) VDD = 12V, RL = 4, 10% THD+N 3.8W (typical)      
  • Shutdown current of 55µA (typical)

About National’s Audio Portfolio
National Semiconductor works with every major handset maker in the world and is the leading provider of audio amplifier systems for the cell phone market.  The company’s line of Boomer audio amplifiers enhances and enriches the entire range of sound – from voice, ring sounds and music – that can be amplified in a mobile phone.  National manufactures Class AB and Class D mono and stereo speaker amplifiers, mono and stereo headphone amplifiers, and audio subsystems for desktop and notebook computers, multimedia displays and portable electronic devices.  The company also offers its higher-power Overture® amplifiers for consumer stereo and home theater systems.  For more information on National’s audio products, visit http://audio.national.com.

Pricing and Availability
Available now in a TO-263 package, the LM4952 is priced at $1.10 in 1,000-unit quantities.  More information on the LM4952 is available at http://www.national.com/pf/LM/LM4952.html. A large selection of audio amplifiers is supported by National’s WEBENCH® online design tool.  To explore these solutions, visit http://webench.national.com.  To learn about high-performance audio amplifiers for portable applications, visit National’s library of online seminars.

About National Semiconductor
National Semiconductor, the industry’s premier analog company, creates high-performance analog devices and subsystems.  National’s leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National’s key markets include wireless handsets, displays, PCs and laptops.  The company’s analog products are also optimized for numerous applications in a variety of electronics markets, including medical, automotive, industrial, and test and measurement.  Headquartered in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004.  Additional company and product information is available at www.national.com
.