TI Home > News Releases

News Releases

Engineers Can Create Thousands of Matched 8-, 10- and 12-Bit Data Converter/Amplifier Combinations with National Semiconductor’s WEBENCH Signal-Path Designer Toolset

Latest WEBENCH Online Design Environment Enables Engineers to Select and Tune Optimal Signal-Path Applications in Minute

Jun 6, 2005

June 6, 2005 - A new WEBENCH® Signal-Path Designer toolset from National Semiconductor Corporation (NYSE:NSM) provides engineers with an easy-to-use tool to select, design and evaluate critical data converter and amplifier/filter components and circuits.
 
National’s expansion of its online design environment pairs its newly released low-power-consumption, general-purpose analog-to-digital converters (ADCs) with its vast portfolio of operational amplifiers to create more than 10,000 optimized signal-path solutions.  To see the tool create an optimized 12-bit, 1 mega-sample per second (MSPS) signal path in two minutes, visit http://webench.national.com/signalpathdemo.

Designing signal paths is a known art form where analog experts select resolution, sampling speed and filtering required by their desired system performance.  The effects of noise, impedance, signal-level matching and power usage all play a significant role. 

“The quality of the signal path is determined by the expertise of the designer and the performance of the components selected,” said Antonio Visconti, product line director of National’s Data Conversion Division.  “National’s Signal-Path Designer tool helps both expert and novice match our newest low-power-consumption ADCs with the best filter and amplifier in a complete design in a matter of minutes.” 

The Signal-Path Designer tool offers an intuitive, step-by-step guide to balance the resolution, speed and power consumption of a performance-matched ADC with the ideal filters, passive components and amplifier to create the optimal performance ADC/amplifier circuit.  The tool also provides filter simulations for both the ideal and device models for comparison purposes. 

"National is dedicated to providing excellent signal-path solutions for our customers," said Phil Gibson, vice president, Corporate Marketing at National Semiconductor.  "National's broad array of ADCs offers the industry's best power consumption in the 50 KSPS to 1 MSPS speed range.  Customers can pair these ADCs with our superior op amps to tailor thousands of designs for their requirements and achieve superior performance in a matter of minutes." 

National’s Unique Data Conversion Portfolio
National Semiconductor offers a broad range of general-purpose and high-speed ADCs ranging from kilo-sample to giga-sample per second sampling rates.  National’s recently announced general-purpose family, available for selection and testing in the WEBENCH Signal-Path Designer toolset, consists of 36 8-, 10- and 12-bit ADCs available in 1-, 2-, 4- and 8-channel configurations.  These ADCs offer guaranteed performance across three speed ranges between 50 KSPS (kilo-samples per second) and 1 MSPS.  They are also pin- and function-compatible within a specific channel configuration, which allows designers to easily migrate across resolutions and speeds.  National’s high-speed data conversion products, with resolutions from 1 MSPS to multiple giga-samples per second, will be added to the WEBENCH Signal Path Designer toolset in the next year. 

A Seamless Suite of Online Tools and Resources
National’s WEBENCH environment eliminates the need for a design engineer to perform tedious hand calculations and includes extensive online tutorials in analog design.  The tools offer instant access to the latest SPICE models, parametric data and package information, enabling designers to simultaneously compare the performance of multiple devices in multiple circuit requirements.  Overnight delivery in the United States is available on all National products with the WEBENCH environment.

The WEBENCH Signal-Path Designer toolset works seamlessly with National’s other WEBENCH tools for power, audio, amplifiers and active filters, including http://Solutions.National.com
and National’s online distance learning facility, Analog University®.  To try any of National’s WEBENCH design tools, go to http://webench.national.com.

Note to editors: High-resolution downloadable screenshots of WEBENCH Signal-Path Designer tools are available on National's photo gallery at http://www.national.com/company/pressroom/gallery/dcs.html
.

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high-performance analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National's key markets include wireless handsets, displays and laptops.  The company's analog products are also optimized for numerous applications in a variety of electronics markets, including medical, automotive, industrial, and test and measurement.  Headquartered in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004.  Additional company and product information is available at www.national.com.