TI Home > News Releases

News Releases

National Semiconductor Introduces 2:1 High-Speed Multiplexer for High-Fidelity Analog Applications

Jun 6, 2005

June 6, 2005 – National Semiconductor (NYSE:NSM) today introduced the LMH6570, a 2:1 high-speed, high-performance analog multiplexer (MUX) designed for professional-grade video and other high-fidelity, high-bandwidth analog applications.  Based on National’s VIP10 process technology, the LMH6570 is ideal for applications requiring very high speed and low distortion, such as video routers, multi-input video monitors, instrumentation and test equipment, multi-channel A/D drivers and picture-in-picture video switches. 

Multimedia and high-definition television (HDTV) applications can benefit from the LMH6570’s 0.1 dB gain flatness of 150 MHz and its 2200 volts per microsecond (V/us) slew rate.  The LMH6570 is optimized for maximum speed and performance in a small-form-factor SOIC package.  It also provides a 400 MHz bandwidth at 2V peak-to-peak output signal levels.

The LMH6570 supports composite video applications with its 0.02 percent and 0.05 degree differential gain and phase errors for NTSC and PAL video signals, while driving a single, back-terminated 75 Ohm load.  An 80 mA linear output current is available for driving multiple video load applications.  The LMH6570’s gain is set by external feedback and gain-set resistors for maximum flexibility.

Additional Features of the LMH6570:

  • 500 MHz, 500 mVpp, -3dB bandwidth, Av=2      
  • 2200 V/us slew rate      
  • 8 ns channel switching time      
  • 0.1 dB gain flatness to 150 MHz       
  • 70 dB channel-to-channel isolation at 10 MHz      
  • Wide supply voltage range: 6V (±3V) to 12V (±6V)       
  • -68 db HD2 at 5 MHz      
  • -84 dB HD3 at 5 MHz      
  • Shutdown pin

About National’s Amplifier Portfolio
Specializing in high-performance amplifiers and comparators, National Semiconductor offers a complete portfolio of op amps ranging from building-block chips to application specific standard products (ASSPs), including precision, high-speed, low-power and low-voltage amplifiers. The company has a long history of innovation in amplifiers, including the first low-voltage op amp and the “amp-in-a-mic.”  National also leads the industry in packaging technology with its revolutionary Silicon Dust™ and micro SMD packaging technologies.  For more information on National’s amplifier products, visit http://amplifiers.national.com

VIP10 Process
National's LMH6570 is National’s newest amplifier created using the VIP10 process.  Developed in National's wafer fabrication site in Arlington, Texas, the VIP10 process is a high-speed, dielectrically isolated, complementary BiCMOS process that utilizes deep trench technology on a bonded wafer for complete dielectric isolation and optimal high-speed amplifier performance.  The VIP10 process technology allows National to design the most power-efficient, performance-oriented high-speed amplifiers on the market today.

Pricing and Availability
Available now in an 8-pin SOIC package, the LMH6570 is priced at $2.15 in 1,000-unit quantities.  Lead-free package options are also available.  More information on the LMH6570 is available at http://www.national.com/pf/LM/LMH6570.html
.  A large selection of amplifiers is supported by National’s Amplifiers Made SimpleSM WEBENCH® online design tool.  To explore these solutions, visit http://webench.national.com. To learn more about designing with amplifiers, visit our library of online seminars.

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high-performance analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National's key markets include wireless handsets, displays and laptops.  The company's analog products are also optimized for numerous applications in a variety of electronics markets, including medical, automotive, industrial, and test and measurement.  Headquartered in Santa Clara, California, National reported sales of $1.98 billion for fiscal 2004, which ended May 30, 2004.  Additional company and product information is available at www.national.com
.