TI Home > News Releases

News Releases

Texas Instruments' new FlatLink™ transmitter offers first glueless connection to low-power embedded processors

LVDS serializer saves up to 83 percent board space and supports HD resolutions

PRNewswire
Aug 10, 2009

DALLAS

(NYSE:TXN)

DALLAS, Aug. 10 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced the first LVDS serializer that connects directly to 1.8-V powered processors. Using TI's FlatLink(™) technology, the SN75LVDS83B eliminates the need for a costly level shifter when using 1.8-V and 2.5-V logic interfaces, lowering cost and reducing board space by up to 83 percent. The SN75LVDS83B supports 8-bit color and serializes RGB data. It then consolidates 24 data lines into one LVDS clock and four LVDS data pairs, which connect to LCD modules. For product details visit: www.ti.com/sn75lvds83b-pr.

The SN75LVDS83B supports applications such as netbooks, mobile Internet devices, digital picture frames and others where an LVDS link from a processor to the LCD module is required. The SN75LVDS83B supports a very broad pixel frequency range from 10 MHz up to high-definition (HD) screen resolutions of 135 MHz. The device is compatible with numerous processors, including OMAP35x applications processors and digital media processors based on TI's DaVinci(™) technology.

Key features and benefits of the SN75LVDS83B

  • Connects directly to any TTL level from 1.8 V to 3.3 V, eliminating the need for additional components
  • Eliminates the level shifter, lowering cost by more than one dollar and reducing board space by up to 83 percent with the BGA package, and up to 39 percent with the TSSOP package
  • 135-MHz pixel clock supports HD screen resolutions

Availability and pricing

The SN75LVDS83B is available now in a 56-pin TSSOP priced at $2.60, and a 56-ball BGA package priced at $2.80. The SN75LVDS83A is available in the 56-pin TSSOP package only. The SN75LVDS83A has a maximum frequency of 100 MHz, supports only 3.3-V input levels and is priced at $2.10. All prices are for quantities of 1,000 units.

Find out more about the SN75LVDS83B/A by visiting these links:

 About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 30 countries. For more information, go to www.ti.com.

Trademarks

DaVinci and FlatLink are registered trademarks of Texas Instruments. All other trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Photo: http://www.newscom.com/cgi-bin/prnh/20010105/NEF016LOGO
SOURCE: Texas Instruments Incorporated

Web site: http://www.ti.com/