TI Home > News Releases

News Releases

National Semiconductor’s Dual Mux-Buffer with Integrated Equalizer Delivers Industry’s Best Signal Integrity

Dual Signal-Conditioning Multiplexer/Repeater Adds Redundancy to Legacy Backplanes and Cost-effective Cables for Data Transfers from 1 Gbps to 4 Gbps

Oct 24, 2005

October 24, 2005 – National Semiconductor Corporation (NYSE: NSM), a leading supplier of high-speed interface devices, today introduced a signal conditioning and repeating product with dual 1:2 and 2:1 multiplexer functions that extend the reach of high-speed switch, router, storage area network (SAN) and server backplanes.  The DS40MB200 can also be used as a redundancy switch in backplanes, and can extend the reach of PCI express connectivity in PCs, security systems and professional video applications.

The DS40MB200 is a dual 1:2 and 2:1 multiplexer with integrated equalizers on every input, configurable pre-emphasis on every output and up to 4 Gbps of serial I/O performance, providing the lowest jitter and longest cable reach in the industry.  In many applications, cost-effective backplanes and cables require equalization and boost to ensure reliable data transfer between the source and destination.  The DS40MB200 is optimized for error-free transmission on more than 80 inches of FR4 backplanes or up to 15 meters of low-cost cables. 

"Similar products on the market today can’t reach the level of jitter performance, pre-emphasis boost or edge rates that National’s DS40MB200 provides," said Jeff Waters, product line director for National Semiconductor’s Interface Division.  “With National’s DS40MB200, our customers can dramatically reduce signal integrity problems when driving signals off-board over long data transmission lines or inexpensive cables.”

The DS40MB200 easily attaches to a field programmable gate-array (FPGA) or application-specific integrated circuit (ASIC) to provide signal path redundancy, signal buffering and improved serial I/O performance on low-cost interconnects.  It features six kilovolts of ESD (electrostatic discharge) immunity.  The high-speed serial inputs feature an integrated receive equalizer to compensate for input transmission line loss.
 
Technical Features of the DS40MB200 Multiplexer/Buffer
The DS40MB200’s high-speed serial inputs feature an integrated equalizer, the outputs feature configurable pre-emphasis, and the input stages have a fixed-equalizer to reduce ISI (inter-symbol interference) distortion from board traces.  The multiplexer/buffer compensates for up to 5 dB of transmission loss.  Each output drive has four configurable steps of pre-emphasis to compensate against transmission losses from long FR4 backplanes.  The pre-emphasis levels can be independently controlled for the line-side and switch-side drivers.  The outputs buffer and condition the signal so that the lower and higher frequencies reach similar amplitudes at the end of the backplane and minimize deterministic jitter.

The two independent channels each contain a transmitter with a fan-out of two and a receiver with a 2:1 input multiplexer.  The multiplexers can be configured to handle system redundancy requirements from the line card to the controller card.  They also can be configured to provide a loop-back function through the device for either device-level or system-level testing.  The internal loop-back paths from switch-side input to switch-side output enable at-speed testing.  All receiver inputs and driver outputs are terminated internally utilizing terminating resistors on-chip. The inputs are compatible to AC-coupled LVDS (low voltage differential signaling), LVPECL (low voltage positive emitter coupled logic) and CML (common mode logic).

For more information on the DS40MB200, to order samples and an evaluation board, or to download an application note, visit http://www.national.com/pf/DS/DS40MB200.html.  An on-demand online seminar, “Boosting FPGA and CPLD Interface Performance for Off-board Data Transmission,” is available for viewing at http://www.national.com/onlineseminar/2005/interface/interface.html.

National’s Interface Products
National Semiconductor, the LVDS technology innovator and market leader, offers a wide range of interconnect solutions that transfer high-speed digital signals using world-class analog technology.  These solutions help system designers develop high-performance applications in a variety of markets, including communication and industrial systems.  The products feature high reliability, low power and low noise, as well as dramatic systems savings in cable and connector costs.  National Semiconductor is the world’s largest supplier of high-speed LVDS products, according to Databean’s 2005 Analog IC Market Share survey.  For more information on National’s interface products, visit http://www.national.com/appinfo/interface/.

Pricing and Availability
Available now and packaged in a 48-pin LLP®, the DS40MB200 is priced at $17.40 in 1,000-unit quantities.

Note to editors:  To view a high-resolution downloadable photo of this product, visit National's photo gallery at http://www.national.com/company/pressroom/gallery/es.html.
 
About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high-value analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions.  National's key markets include wireless handsets, displays and a variety of broad electronics markets, including medical, automotive, industrial, and test and measurement applications.  Headquartered in Santa Clara, California, National reported sales of $1.91 billion for fiscal 2005, which ended May 29, 2005.  Additional company and product information is available at www.national.com.