TI Home > News Releases

News Releases

National Semiconductor Introduces Industry's First Extended Temperature LVDS Transmitter and Receiver Family

LVDS Transmitters, Receivers Deliver 400 Mbps of Performance in Extreme Environments

Jan 30, 2006

January 30, 2006 – National Semiconductor Corporation (NYSE:NSM) today introduced five new extended temperature single and dual transmitters and receivers to the company’s industry-leading portfolio of low-voltage differential signaling (LVDS) products.  The general-purpose LVDS physical layer devices (PHYs) are optimized for driving signals through cable harnesses in systems operating in harsh, high-temperature environments, such as automotive, industrial and military applications.

The DS90LV011AH transmitter, DS90LT012AH receiver, DS90LV027AH dual transmitter, DS90LV028AH dual receiver and DS90LV049H integrated dual transceiver are guaranteed to operate in environments up to 125 degrees C.  Operating at very low power, the five new products deliver superior LVDS performance characteristics, data rates up to 400 Mbps and excellent noise immunity.

"Designers of high-performance industrial systems were once limited to lower-speed communication standards like RS-485 and CAN for data transport,” said Jeff Waters, product line director for the Interface division at National.  “National’s new extended temperature LVDS PHYs will enable ten times the level of performance of lower-speed communication standards, driving data rates up to 400 Mbps over cables in very hot and electro-magnetically noisy environments.”

In a typical application, the LVDS PHYs improve signal integrity by translating the single-ended control and data signals from sensors into LVDS signals for transmitting to the digital processor, typically an FPGA or ASIC.  In automotive or industrial systems where electrical noise is often unavoidable, LVDS is the best signaling technology choice because of its superior noise immunity and error-free performance.

Technical Features of the Extended Temperature LVDS PHYs
The five new extended temperature single and dual transmitters and receivers support the differential LVDS interface standard from -40 degrees C to +125 degrees C.  The DS90LV011AH transmitter, DS90LT012AH receiver, DS90LV027AH dual transmitter, DS90LV028AH dual receiver and DS90LV049H integrated dual transceiver functions use the LVDS analog interface to provide a high-performance signal path that transfers digital information.  In addition, the DS90LT012AH features an integrated LVDS input termination to save board space.  The DS90LV027AH and DS90LV028AH feature a flow-through pin-out to simplify board layout.

All of the LVDS PHYs are offered in extremely small packages to minimize board space.  The DS90LV011AH and DS90LT012AH are packaged in a 5-pin SOT-23.  The DS90LT012AH is also available as a bare die.  The DS90LV027AH and DS90LV028AH are packaged in an 8-pin SOIC and the DS90LV049H is packaged in a 16-pin TSSOP.  Lead-free package options are also available. 

For more information on the LVDS PHYs or to order samples, visit http://www.national.com/pf/DS/DS90LV011AH.html, http://www.national.com/pf/DS/DS90LT012AH.html, http://www.national.com/pf/DS/DS90LV027AH.html, http://www.national.com/pf/DS/DS90LV028AH.html, http://www.national.com/pf/DS/DS90LV049H.html

For more information on National’s interface products, visit http://lvds.national.com.

About National’s Interface Products
National Semiconductor, the LVDS technology innovator and market leader, offers a wide range of interconnect solutions that transfer high-speed digital signals using world-class analog technology.  These solutions help system designers develop high-performance applications in a variety of markets, including communication and industrial systems.  The products feature high reliability, low power and low noise, and dramatic systems savings in cable and connector costs.  National Semiconductor is the world’s largest supplier of high-speed LVDS products, according to Databean’s 2005 Analog IC Market Share survey.

Pricing and Availability
Available now in 1,000-unit quantities, the DS90LV011AH is priced at 46 cents each, the DS90LT012AH is 38 cents each, the DS90LV027AH is 78 cents each, the DS90LV028AH is $1.08 each and the DS90LV049H is 90 cents each. 

Note to Editors:  To view a high-resolution downloadable photo of these products, visit National's photo gallery at http://www.national.com/company/pressroom/gallery/network.html.

About National Semiconductor
National Semiconductor, the industry's premier analog company, creates high-value analog devices and subsystems.  National's leading-edge products include power management circuits, display drivers, audio and operational amplifiers, communication interface products and data conversion solutions. National's key analog markets include wireless handsets, displays and a variety of broad electronics markets, including medical, automotive, industrial, and test and measurement applications. Headquartered in Santa Clara, California, National reported sales of $1.91 billion for fiscal 2005, which ended May 29, 2005.  Additional company and product information is available at www.national.com
.