TI Home > News Releases

News Releases

Texas Instruments' latest operational amplifier provides industry's lowest noise, distortion and quiescent current

Dual-channel, bipolar-input amplifier delivers leading sound in pro audio applications

PRNewswire
Sep 14, 2009

DALLAS, Sept. 14 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced the industry's highest performance dual-channel, bipolar-input audio operational amplifier. The OPA1612, from TI's Burr-Brown Audio line, offers designers 60 percent less noise and 50 percent lower distortion as compared to competitive devices, resulting in clear, crisp sound. The amplifier supports multiple channels without significant power consumption in applications such as professional audio and broadcast studio equipment, microphone pre-amplifiers, analog and digital mixing consoles, high-end A/V receivers and audio test and measurement equipment. For details about this product, please see www.ti.com/opa1612-pr.

 

Key features and benefits of the OPA1612

  • Bipolar input achieves very low 1.1-nV square root Hz noise density with an ultra-low distortion of 0.000015 percent at 1 kHz to enable clear, crisp audio
  • Rail-to-rail output swing to within 600 mV with a 2 K Ohm load increases headroom and maximizes dynamic range
  • Widest supply operation range of +/-2.25 V to +/-18 V from only 3.6 mA of supply current per channel provides excellent dynamic behavior over a wide range of load conditions
  • Independent circuitry delivers lowest crosstalk and freedom from interactions between channels, even when overdriven or overloaded
  • Seamless connectivity to TI audio converters (PCM17xx and PCM16xx) and microphone preamplifiers (PGA2500 and PGA2505) reduces time-to-market

 

Availability and pricing

The OPA1612 is available today in an SO-8 package for $2.75 in 1,000-unit quantities. The OPA1611 single-channel device is also available today in an SO-8 package at $1.75.

 

Find out more about TI's amplifier and signal chain portfolio by visiting the links below:

 

About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.

 

Trademarks

All trademarks and registered trademarks are property of their respective owners.

 

 

SOURCE Texas Instruments Incorporated

Photo: http://www.newscom.com/cgi-bin/prnh/20010105/NEF016LOGO
http://photoarchive.ap.org
PRN Photo Desk photodesk@prnewswire.com

SOURCE: Texas Instruments Incorporated

Web site: http://www.ti.com/