TI Home > News Releases

News Releases

Texas Instruments introduces lowest cost DSP development tool at $49 with full emulation capabilities and extensive development environment

New eZdsp™ USB stick eases creation of audio, voice, medical and other portable applications

PRNewswire
Sep 16, 2009

HOUSTON, Sept. 16 /PRNewswire/ -- For many designers, the cost and time to set up development tools is a major barrier when evaluating a new digital signal processor (DSP) platform. To lower this barrier, Texas Instruments Incorporated (TI) (NYSE: TXN) today announced the availability of the TMS320VC5505 eZdsp USB stick development tool, which drops the cost of a full-featured emulator and integrated development platform down to $49. This enables rapid creation of DSP applications including portable audio players, voice recorders, IP phones, portable medical devices, biometric USB keys, software defined radios (SDRs), hands-free headsets and metering applications. At this extremely low price point, it is the industry's lowest cost DSP tool, making development accessible to existing and potential customers, hobbyists, researchers and students. (www.ti.com/c5505ezdsp-prprod).

Comparable to the size of a stick of gum, the C5505 eZdsp stick simplifies development by providing integrated features such as an on-board XDS100 emulator and on-board audio codec and connectors. Taking advantage of the energy efficient C5505 DSP, the eZdsp requires no other components or cables allowing the entire development tool to be powered by the USB port. Designers simply plug into the USB port of any laptop or workstation for hassle-free development and a simple out-of-the-box experience.

TI will offer training and demonstrations of the C5505 eZdsp USB stick at ESC Boston on September 23 in room 204 from 1:15 p.m. - 2:45 p.m.

C5505 eZdsp USB stick development tool key features and benefits:

  • Based on the C5505 processor, the industry's lowest power 16-bit DSP with active power consuming less than 0.15 mW/MHz and standby power less than 0.15 mW
  • Low price point at $49 eliminates cost concerns or barrier to entry
  • Integrated XDS100 emulator provides complete debug capabilities and visibility inside the processor for algorithm optimization and benchmarking
  • On-board audio codec and connectors allow developers to evaluate many features of the C5505 processor and quickly optimize complex DSP algorithms in terms of performance and power consumption across a variety of design scenarios
  • Extension connector allows developers to design and directly connect to daughter cards suitable for their application
  • Unique form factor plugs into any laptop or workstation, conserving test bench space
  • Simplifies development tools setup by eliminating power and interface cables
  • Includes the complete Code Composer Studio™ version 4 integrated development environment (IDE) free of charge
  • Stereo line in and headphone out connectors making it possible to evaluate many DSP algorithms and listen to them
  • Users can easily migrate to TI's C5505 evaluation module that offers additional extensive evaluation options
  • Makes DSP evaluation and development easy and accessible

Pricing and availability

The feature-rich C5505 eZdsp USB stick development tool is available now at the low cost of USD $49, which includes a full XDS100 emulator and a target version of the industry-leading CCStudio v.4. Special incentives are available for educators, university students and developers actively participating in TI's online community.

The C5000 platform is supported by TI's extensive Developer Network, as well as a complete chip support library, comprehensive application notes, reference designs, application guides, videos and online communities.

Find out more about TI's extensive C5505 eZdsp USB stick and C5505 DSP portfolio by visiting the links below:

About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.

Trademarks

Code Composer Studio is a trademark of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Photo:

http://www.newscom.com/cgi-bin/prnh/20010105/NEF016LOGO
http://photoarchive.ap.org

PRN Photo Desk photodesk@prnewswire.com

SOURCE: Texas Instruments Incorporated

Web site: http://www.ti.com/