TI Home > News Releases

News Releases

National Semiconductor Acquires Act Solar, Extending Its Solar Energy Efficiency and Management Capabilities

Mar 19, 2009

March 19, 2009 -- National Semiconductor Corp. (NYSE:NSM) announced today it has acquired Act Solar, Inc. a privately held solar energy company that provides power optimization solutions for commercial and utility-scale solar installations.

With the acquisition of Act Solar, National expands its portfolio of power optimization technologies along with the acquisition of new diagnostics and panel monitoring capabilities for solar arrays.

“National Semiconductor is applying its ‘PowerWise’ capabilities to drive new energy generation and efficiency initiatives in the solar panel marketplace,” said Mike Polacek, senior vice president of National’s Key Market Segments. “Now with Act Solar we can further improve the performance and efficiency of solar systems, at the same time providing monitoring capabilities not available before. This will make solar installations more efficient and ultimately reduces the cost of solar energy for everyone.”

National’s SolarMagic™ technology enhances the efficiency and output of solar arrays when the panels are affected by mismatch issues including shade, debris, different panel types, and panel aging. Panel mismatch can disproportionately impact the output of a solar installation. For example, an entire solar array’s energy output can be reduced by half if just 10 percent of one solar panel is shaded by a tree, chimney or rooftop vent. Recent internal testing showed that National’s SolarMagic power optimizers recovered 57 percent of power lost due to shade, thereby enhancing the solar installation’s output and efficiency. SolarMagic power optimizers begin shipping this spring.

Act Solar now becomes part of the SolarMagic family. Its products improve array performance by 6 to 11 percent using patent-pending technology, complementing central inverters by dynamically re-circulating small amounts of energy as needed. The balance of the array is maintained, assuring maximum power output. The technology utilizes a revolutionary technique for power tracking, which works by injecting energy into the string as opposed to traditional DC-DC voltage converting approaches. Early field tests and historical modeling have shown that this solution can cumulatively deliver 40 to 80 percent more power over the operating life of a solar panel installation.

About National Semiconductor
National Semiconductor creates energy-efficient analog and mixed-signal semiconductors. Its PowerWise® products enable systems that consume less power, extend battery life, and generate less heat. Headquartered in Santa Clara, Calif., National reported sales of $1.89 billion for fiscal 2008 which ended May 25, 2008. Additional company and product information is available at www.national.com.

About Act Solar
Act Solar is a power management technology company that provides optimization solutions for solar installations. Its flagship product, PowerString™, improves the performance, operation and longevity of solar power plants. Headquartered in Santa Clara, California, Act Solar was founded in 2006 by an experienced team of Silicon Valley professionals focused on making solar arrays more productive, competitive, and a mainstream source of energy in the world market. For more information, visit: www.actsolar.com.