TI Home > News Releases

News Releases

SolarMagic Retrofit of Affordable Housing Project Increases Energy Harvest by 22.6 Percent

National Semiconductor’s Power Optimizers Reduce Annual Energy Costs for California’s Affordable Housing Development

Jul 13, 2009

OAKLAND, Calif. – July 13, 2009 – National Semiconductor Corp. (NYSE:NSM), of Santa Clara, Calif., today announced the retrofit of an affordable housing project in Oakland with its industry award-winning SolarMagic™ power optimizers, boosting the electricity production by 22.6 percent. The 30-kilowatt solar system sits atop the Oak Street Terrace, a 39-unit affordable housing development specifically designed for low-income seniors.

Completed in 2005, the multi-story apartment building was initially designed to be as energy efficient and eco-conscious as possible, and is constructed out of recycled and natural building materials. Jigar Shah, solar visionary and founder of SunEdison, installed the solar system and is providing the power generated through a power purchase agreement, where residents lock into a low, fixed-rate for electricity.

"For over four years, our Oak Street installation has been helping residents pay less for electricity, and the addition of SolarMagic has dramatically boosted system performance," said Jigar Shah. "SolarMagic is helping us get 22.6 percent more power out of the same panels, making the system even more productive and cost-effective.”

Due to environmental and system efficiency factors, all solar installations provide less energy than the maximum rated output of the solar modules. This difference is called the "performance ratio." The industry average performance ratio is 75 percent to 80 percent. After a period of monitoring and evaluation, National Semiconductor found the performance ratio of the Oak Street site had degraded since installation from 77 percent to 67 percent.

While the site was equipped with a state-of-the art monitoring system, National Semiconductor found that there was an unrealized gain of 20,000 kilowatt hours. In March 2009, National optimized the system performance and retrofitted approximately one-third of the 204-panel system with SolarMagic power optimizers. Subsequently, the performance ratio of the site improved to 82 percent, an overall improvement in power output of 22.6 percent -- well in excess of its forecast production rate. The detailed case study can be downloaded at http://www.solarmagic.com/vcm/SolarMagic_Content/files/en_US/SolarMagic_CaseStudy_OakStreet.pdf.

“Real world conditions such as shade, aging and panel mismatch can significantly degrade the performance of a photovoltaic system,” said Ralf Muenster, director of National Semiconductor’s Renewable Energy Segment. “With National’s SolarMagic power optimizers, the true potential of these systems can be realized.”

SolarMagic power optimizers first hit the market in May 2009, and since then, National Semiconductor has announced the initiation of further field trials with SunEdison. For more information, visit www.solarmagic.com.

National will demonstrate its SolarMagic power optimizers at its Intersolar North America booth (#8656). The conference and exhibition at the Moscone Center in San Francisco, runs July 14-16, 2009. As part of the conference, Ralf Muenster will make a presentation, “Off-grid Systems - Technological Advancements,” on Wednesday, July 15 at 3:45 p.m. More information on the conference is available at http://bit.ly/IntersolarUS.

Note to editors: To download video B-roll of the Oak Street SolarMagic retrofit, visit National's photo gallery at http://www.solarmagic.com/news_events#pressvideos.

About National Semiconductor
National Semiconductor is a leader in analog power management technology. Its products include easy-to-use integrated circuits, PowerWise products that enable more energy-efficient systems, and SolarMagic products which improve the energy output of solar arrays. The company celebrates its 50th anniversary this year. Headquartered in Santa Clara, Calif., National reported sales of $1.46 billion for fiscal 2009. Additional information is available at www.national.com.