TI Home > News Releases

News Releases

National Semiconductor Introduces Industry’s First PMBus System Power Management and Protection IC

LM25066 Reduces Data Center Operating Expenses, Improves System Reliability

Feb 23, 2010

Feb. 23, 2010 – National Semiconductor Corp. (NYSE:NSM) today announced the industry’s first system monitoring, protection and control integrated circuit (IC) with on-chip power management bus (PMBus) support. The LM25066 provides designers of blade servers, storage networking systems, routers/switches and modular subsystems with a solution that improves system reliability and reduces operating expenses in data centers.

National’s LM25066 integrates high-performance monitoring, protection and control blocks that precisely control and manage the electrical operating conditions of each blade in the chassis. It also provides accurate monitoring of critical system power consumption and fault conditions. National’s power management experts will demonstrate the LM25066 in National’s booth #332/334 at the Applied Power Electronics Conference (APEC) in Palm Springs, Calif.

The LM25066 continuously supplies the system management host with real-time power, voltage, current, temperature and fault data for each blade subsystem. The LM25066’s system management bus (SMBus) communications interface delivers this data using the PMBus protocol. The host’s system diagnostic and optimization routines use the data to increase system reliability and minimize the data center’s total power consumption.

Key Features - LM25066 PMBus System Power Management and Protection IC
The LM25066 features a voltage input range of 2.9V to 17V and a selectable 25 mV/50 mV current limit threshold for addressing a wide range of intermediate bus voltages and load currents. The LM25066 monitoring block measures both current and voltage at 1,000 times per second with a current measurement accuracy of three percent over the full temperature range of -40 degrees C to 125 degrees C. Additionally, its simultaneous sampling of current and voltage provides a true power measurement of the server blade power consumption. The monitoring block also captures the peak current and peak power and computes the average of subsystem operating parameters (Vin, Iin, Pin and Vout).

A temperature monitoring block on the LM25066 interfaces with a low-cost external diode for monitoring the temperature of the external MOSFET or other critical temperature source. The LM25066 reports the status of all system parameters and fault conditions through the SMBus interface and offers individually programmable warning thresholds for all faults. This feature provides design flexibility and dynamic system protection.

The LM25066 control and protection blocks include National’s unique hot-swap architecture that provides both current and power limiting to protect sensitive circuitry during insertion of boards from a live system backplane or any other "hot" power source. The LM25066 protection block also provides adjustable under/overvoltage and hysteresis.

National supports the LM25066 with a suite of powerful development tools that simplify application design and system verification. System designers may also use these tools to create value-added features for their subsystems.

Pricing and Availability
The LM25066 is supplied in a 4 mm by 5 mm, 24-lead LLP® package and is priced at $5.95 each in 1,000-unit quantities. The LM25066 is sampling now with full production volumes expected in the second quarter of 2010. For more information or to order samples and an evaluation board, visit www.national.com/pf/LM/LM25066.html.

Note to editors: To view a high-resolution downloadable photo of this product, visit National's National's photo gallery.

About National Semiconductor
National Semiconductor is a leader in analog power management technology. Its products include easy-to-use integrated circuits, PowerWise products that enable more energy-efficient systems, and SolarMagic products which improve the energy output of solar arrays. The company celebrated its 50th anniversary last May. Headquartered in Santa Clara, Calif., National reported sales of $1.46 billion for fiscal 2009. Additional information is available at www.national.com.