TI Home > News Releases

News Releases

New 10 Gbps Repeaters from National Semiconductor Double Signal Conditioning Performance at Half the Power

Repeaters Extend Cable Reach, Reduce Interconnect Cost in Data Center Systems

Jan 27, 2011

January 27, 2011 – Extending its leadership in high-performance analog technology, National Semiconductor Corp. (NYSE: NSM) today announced three multi-channel PowerWise® 10 Gbps repeaters that provide the industry’s highest equalization gain (36 dB), consume half the power (55 mW/channel) and deliver twice the reach (20 meters over 24-AWG cable) of current industry solutions.

Powered by National’s third-generation SiGe BiCMOS process, National’s 10 Gbps repeater family extends interconnect reach and enables higher data bandwidth up to 10.3125 Gbps by performing both receive equalization and transmit de-emphasis to compensate for channel loss in data center and high-performance communication systems. Target applications include high-speed active cable assemblies and FR-4 backplanes using serial protocols such as 10 GbE, Fibre Channel, XAUI, CPRI and Infiniband. The repeaters also support SAS/SATA out of band (OOB) signaling for storage applications.

The explosion of multimedia content on the Internet, cloud computing, and the advent of multi-core virtualized servers are pushing interface bandwidth requirements in modern data center systems. However, interconnect length remains the same, posing power and signal integrity issues. National’s signal conditioners embedded inside the active copper cable assemblies and backplane boards ensure signal integrity, reduce system power consumption and lower interconnect cost compared to optical alternatives.

National’s 10 Gbps repeaters enable these active copper solutions to consume 4x lower power and 2x longer reach than competitive cabling solutions through the use of a new SiGe BiCMOS process, which produces high bandwidth and low noise transistors that enable low jitter and ultra-low power. The quad DS100BR410 is well-suited for high density connectors such as QSFP and CXP, while the DS100BR111 is designed for single lane SFP+ connectors.

National’s 10 Gbps Repeater Family
The DS100BR410 includes four unidirectional channels and delivers 55 mW/channel typical power consumption, while supporting a 2.5V single-supply voltage. It extends interconnect reach by performing both receive equalization (up to 36 dB boost) and transmit de-emphasis (-9 dB) on each of its channels to compensate for channel loss. This allows for maximum flexibility in physical placement within a system.

The DS100BR210 with two unidirectional channels and the DS100BR111 with one bidirectional lane (one transmit, one receive channel) feature 65 mW per channel typical power consumption and support 3.3V and 2.5V supplies. Both devices perform receive equalization up to 36 dB gain and transmit de-emphasis of -12 dB. All three repeaters allow powering down of unused channels, and apply signal conditioning settings via pin setting or SMBus (I2C compliant).

For more information on National’s 10 Gbps repeater family, please visit http://www.national.com/datacom. To see a video demonstration of active copper cables, visit http://tinyurl.com/ActiveCopper.

Pricing and Availability
Available now, the DS100BR410 is offered in a 7 mm by 7 mm, 48-pin leadless LLP® package and is priced at $13 in 1,000-unit quantities. The DS100BR210 and DS100BR111 will be sampling in early March 2011 and are offered in 4 mm by 4 mm, 24-pin LLP packages with pricing at $6.95 each, both in 1,000-unit quantities.

For more information or to order samples and an evaluation board, visit www.national.com/pf/DS/DS100BR410.html, www.national.com/pf/DS/DS100BR210.html and www.national.com/pf/DS/DS100BR111.html.

Note to editors: To view a high-resolution downloadable photo of these products, visit National's photo gallery at www.national.com/analog/pressroom/interface.

About National Semiconductor
National Semiconductor is a leader in power management technology. Known for its easy-to-use analog integrated circuits and world-class supply chain, National’s high-performance analog products enable its customers’ systems to be more energy efficient. Headquartered in Santa Clara, Calif., National reported sales of $1.42 billion for fiscal 2010. Additional information is available at www.national.com.