TI Home > News Releases

News Releases

Texas Instruments announces new 720 MHz OMAP3530 processor targeted at multimedia applications

Speed upgrades on both the ARM® Cortex™-A8 and TMS320C64x+™ DSP give designers more headroom to add features and custom software

PRNewswire
Sep 29, 2009

HOUSTON, Sept. 29 /PRNewswire/ -- Giving designers more performance to run new application features and additional headroom to add their own IP, Texas Instruments Incorporated (TI) (NYSE: TXN) today announced a speed upgrade for the OMAP3530 applications processor and evaluation module (EVM). The new OMAP3530 processor features a 720 MHz ARM® Cortex™-A8 core and a 520 MHz TMS320C64x+™ DSP. This enables users to gain faster access to databases, spreadsheets, presentations, e-mail, audio and video attachments, Web browsing and video conferencing applications. This single-chip solution also supports faster boot times suitable for applications such as portable infotainment, Point-of-Sale (POS) devices, Web tablets and single board computers (http://www.ti.com/OMAP3530perf-increase-prprod).

720 MHz OMAP3530 processor key features and benefits:

  • 720 MHz ARM Cortex-A8 core provides 1400 Dhrystone million instructions per second (MIPS)
  • 520 MHz C64x+™ DSP provides more headroom to optimize quality audio and video codecs and custom IP
  • POWERVR SGX™ subsystem for 3D graphics acceleration to support display and gaming effects
  • Comprehensive power and clock-management scheme that enables high-performance, low-power operation and low-power standby features
  • Pin-for-pin compatible with TI's OMAP35x devices makes it easy for OEMs to efficiently create a complete product portfolio based on the single platform

OMAP3530 EVM key features and benefits:

  • Based on the 720 MHz OMAP3530 processor and can also be used to evaluate the OMAP3503, OMAP3515 and OMAP3525
  • Ability to run full-featured operating systems, such as Windows® Embedded CE and Linux
  • New S-Video/Component/Composite input, S-Video output
  • Features TI's TVP5146 analog-to-digital video decoder
  • TI integrated power management ICs, OMAP3530 power requirements and design considerations: www.ti.com/omap3530power-pr.

Availability

The OMAP3530 at 720 MHz, available in multiple package size options, as well as the OMAP3530 EVM are now available at www.ti.com/omap35x. In addition to the new 720 MHz devices, developers can continue to take advantage of the OMAP3530 at 600 MHz.

Find out more about TI's OMAP3530 processor and EVM by visiting the links below:

About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.

Trademarks

TMS320C64x+ and C64x+ are trademarks of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Photo:

http://www.newscom.com/cgi-bin/prnh/20010105/NEF016LOGO
http://photoarchive.ap.org

PRN Photo Desk photodesk@prnewswire.com

SOURCE: Texas Instruments Incorporated

Web site: http://www.ti.com/