TI Home > News Releases

News Releases

TI introduces industry's first 800-mA, 30-V linear battery chargers with automatic USB detection

Tiny single-input, single-cell Li-Ion chargers simplify charging in portable designs

PRNewswire
Oct 12, 2009

 DALLAS, Oct. 12 /PRNewswire/ -- Texas Instruments Incorporated (TI) today introduced two families of 800-mA USB battery chargers with automatic USB detection for single-cell, lithium-ion (Li-Ion) battery-powered electronics. The bq2404x and bq2405x battery charger integrated circuits have a high input-voltage range of up to 30 V, and 6.6-V overvoltage protection to support handheld devices, from entry-level feature phones to smartphones, and other low-power handheld devices, that may use low-cost adapters. See: www.ti.com/bq2404x-pr, www.ti.com/bq2405x-pr.

The bq2405x's automatic USB detection feature can intelligently detect if a power source is a dedicated power adapter or USB port. This allows a system to start immediate fast charging if a USB transceiver is unavailable due to a discharged battery.

Key features of the bq2404x and bq2405x battery chargers:

  • Charging accuracy: one percent charge voltage and 10 percent current accuracy using single-output channel
  • USB compliance: USB current limiting and input voltage dynamic power management
  • System safety: complies with JEITA guidelines; 30-V input rating and overvoltage protection and includes a 10-hour safety timer
  • System flexibility: bq2405x has automatic input source detection of USB port or a dedicated power adapter 

Availability and pricing

TI's bq24040, bq24041, bq24050, bq24052 and bq24055 are available in volume now from TI and its authorized distributors. The devices come in two small package options: a 10-pin, 2 mm x 2 mm, or 12-pin, 2 mm x 3 mm SON package. Suggested resale pricing is $1.15 to $1.45 in 1,000-unit quantities. Samples, evaluation modules and application notes on TI's battery chargers are available.

New battery charger selection tool helps speed selection process

TI provides a broad range of battery charger ICs that support single-cell and multi-cell battery packs used in handheld, portable medical and portable industrial equipment. Designers can select recommended products using TI's new Battery charger selector tool, where one can choose criteria based on battery chemistry, number of cells, topology needed and battery voltage levels.

Find out more about TI's battery charging portfolio and other power management products by visiting the links below:

 About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.

Trademarks

All trademarks and registered trademarks are property of their respective owners.

SOURCE: Texas Instruments Incorporated

Web site: http://www.ti.com/