TI Home > News Releases

News Releases

TI delivers industry's first true 0.9 volt microcontroller to drive innovation in smaller, more cost-effective products in consumer electronics, security and more

MSP430L092 MCU enables multiple applications to run from a single-cell battery and offers developers increased flexibility with programmable analog building blocks

PRNewswire
Sep 14, 2010

DALLAS, Sept. 14 /PRNewswire/ -- Driving smaller, lower cost products that run from a single-cell battery, Texas Instruments Incorporated (TI) (NYSE: TXN) today announced the industry's first true 0.9-V microcontroller (MCU) as the newest addition to the ultra-low-power MSP430™ MCU portfolio. Unlike existing MCUs that claim 0.9-V technology, TI's MSP430L092 MCU inherently operates at 0.9-V, including the entire analog and digital logic. Because it operates at 0.9-V, the MSP430 MCU does not require an on-board boost converter, lowering the entire system's power consumption and reduces the need for external circuitry required by traditional solutions. This allows developers to run applications such as electric toothbrushes, razors, toys and security devices off of a single-cell battery, ranging from AAA to coin cell. MSP430L092 also offers programmable analog building blocks that can be configured as five different peripherals. In addition to free software, comprehensive application notes, code libraries and community support, new tool kits are available to help developers fully leverage the benefits of this industry-first device. For more information, please visit www.ti.com/lowvoltagewiki-pr .  

Key features and benefits of the MSP430L092

  • Three 0.9-V MCU variations – MSP430L092 (RAM), MSP430C091 (ROM) and MSP430C092 (ROM) – with up to 2KB RAM and 2KB ROM  provide multiple choices for a path to production
  • Integrated Analog Functions Pool (A-POOL) can serve as an analog-to-digital converter (ADC), digital-to-analog converter (DAC), system voltage supervisor (SVS), temperature sensor or comparator, eliminating the need for external components to reduce overall bill of materials
  • Programmable A-POOL enables the various analog peripheral configurations to run sequentially without user interaction, providing increased flexibility
  • Tool kits, including external EEPROM, and ROM-flow process guide help rapidly move from development to final production
  • Ultra-low-power consumption of 45 microamps (active) and wake-up time of less than 5 microseconds combined with true 0.9-V operation, enable optimized battery usage

 

Pricing and availability

The new MSP430L092 MCUs are priced from $0.85 at 10K units. The supporting MSP-TS430L092 ($99) and MSP-FET430U092 ($149) development tools are immediately available to customers. Tools and silicon can be ordered at www.ti.com/l092-pr-es.  

TI's broad portfolio of MCUs and software

From general purpose, ultra-low power MSP430 MCUs, to Stellaris® Cortex™-M3-based 32-bit MCUs and high performance, real-time control TMS320C2000™ MCUs, TI offers the broadest range of microcontroller solutions. Designers can accelerate time to market by tapping into TI's complete software and hardware tools, extensive third-party offerings and global technical support.

Find out more about TI's MSP430L092 MCUs by visiting the links below:

 

About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun.  A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries.  For more information, go to www.ti.com.

Trademarks

MSP430 is a registered trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated