TI Home > News Releases

News Releases

TI's OMAP4470 apps processor: It's all about the user experience

Latest OMAP™ 4 platform processor sets new standard for mobile computing, bringing up to QXGA display resolution, HD UIs and 2x Web browsing performance

Jun 2, 2011

TAIPEI, Taiwan, June 2, 2011 /PRNewswire/ -- COMPUTEX -- Building on the OMAP™ 4 platform family's technological achievements , Texas Instruments Incorporated (TI) (NYSE: TXN) introduced today the power-efficient OMAP4470 applications processor, designed to deliver the perfect balance between processing power, graphics, display subsystem functionality and multilayered user interface (UI) composition. The multicore OMAP4470 processor surpasses current market solutions with clock speeds up to 1.8 GHz, an 80 percent increase in Web browsing performance, increased memory bandwidth, a 2.5x boost in graphics functionality—via the POWERVR™ SGX544 core from Imagination Technologies—and a unique hardware composition engine. Mobile computing and gaming applications running on operating systems such as Android, Linux and the next version of Microsoft Windows will benefit from the OMAP4470 processor's enhanced capabilities. Customers designing ultrathin laptops, tablets or smartphones around previously released OMAP 4 processors gain the added benefit of pin-to-pin hardware and software compatibility for maximum re-use and faster time-to-market.  

(Photo:  http://photos.prnewswire.com/prnh/20110602/LA12487)

"Superior mobile computing relies on a user experience that dwarfs all others. Fast and crisp Web browsing, HD and liquid UIs, support for the latest applications—these are the elements consumers judge and buy their devices on. The OMAP4470 processor delivers the maximum experience possible with an unmatched, power-efficient architecture," said Remi El-Ouazzane, vice president, OMAP platform business unit, TI.

Making HD UIs a reality  

Courtesy of its advanced graphics architecture, OMAP4470 enables customers to leverage tomorrow's leading-edge display technology by supporting resolution up to QXGA (2048x1536). The new applications processor drives still more unparalleled HD UIs with simultaneous support for up to three HD screens and up to 2x more layered imaging and video composition than competitive solutions—a capability required by the sophisticated UIs of next generation operating systems. This feature is enabled by the combination of a hardware composition engine with a dedicated 2D graphics core, a highly sophisticated display subsystem, and dual-channel LPDDR2 memory enabling up to 7.5 GB/s of throughput to composite the graphics and/or video data output. This frees the GPU to perform graphics-intensive tasks such as gaming or widget creation while the compositing process is assigned to more power-efficient hardware subsystems.

Powerful enough for desktop applications yet highly power-efficient for mobile applications, Imagination Technologies' POWERVR SGX544 GPU complements the OMAP 4 platform's promise of high performance, low power. The OMAP4470 processor is the first OMAP offering to leverage the POWERVR SGX544. Combining the SGX544's features with the sophisticated OMAP architecture enables TI customers to deliver a new set of applications to end-users, including DirectX-driven games and videos.

"Graphics processing is now at the very heart of the mobile computing experience, providing the gateway to an enriched experience of user interface, gaming, location services, web and media," said Hossein Yassaie, CEO, Imagination Technologies. "Combining the OMAP 4 platform's low-power, high-performance architecture with the extensive acceleration capabilities and API support of Imagination's POWERVR SGX544 will enable experiences that will really make people sit up and take notice."

OMAP4470 applications processor features and benefits*



Two ARM® Cortex™-A9 MPCores™ running up to 1.8GHz per core

80% increase in Web browsing performance

Two ARM Cortex-M3 cores  

Smart multicore processing optimized for low-power and real-time responsiveness

SGX544 graphics core

2.5x overall graphics performance increase; support for DirectX, OpenGL ES 2.0, OpenVG 1.1, and OpenCL 1.1

Hardware composition engine with dedicated 2D graphics core

Frees GPU to manage intensive tasks; maximizes power-efficiency

Display subsystem

Supports as many as three HD displays and up to QXGA (2048x1536) resolution; HDMI supporting stereoscopic 3D

Dual-channel, 466 MHz LPDDR2 memory

Higher memory bandwidth enables rendering and compositing of multilayer content at high resolutions

Complete pin-to-pin hardware and software compatibility

Rapid transition and maximum re-use of investment from OMAP4430 and OMAP4460 processors

*Comparative data relative to the OMAP4430 processor


The 45nm OMAP4470 processor is expected to sample in the second half of 2011, with devices expected to hit the market in first half 2012. These products are intended for high-volume mobile OEMs and ODMs, and are not available through distributors.

About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun.  Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities.  This is just the beginning of our story.  Learn more at www.ti.com.


OMAP is a registered trademark of Texas Instruments Incorporated.  ARM is a registered trademark, and Cortex is a trademark of ARM Ltd.  All other trademarks and registered trademarks belong to their respective owners.


SOURCE Texas Instruments Incorporated