TI Home > News Releases

News Releases

BIG performance, SMALL cells: Texas Instruments unleashes industry's most complete small cell base station solutions with dual-mode support and comprehensive software suite

- Comprehensive hardware and software solution drives integration and development efficiencies to record levels

- TMS320TCI6612 and TMS320TCI6614 SoCs are highest performing devices for metro, pico and enterprise base stations

- Dual-mode support eases operators' migration from 3G to 4G; simultaneous LTE and WCDMA support reduces OPEX and CAPEX costs

PRNewswire
Jun 20, 2011

LONDON, June 20, 2011 /PRNewswire/ -- FEMTOCELLS WORLD SUMMIT -- Texas Instruments Incorporated (NYSE: TXN) (TI) today unveiled the TMS320TCI6612 and TMS320TCI6614, the industry's most comprehensive System-on-Chips (SoCs) for developers of metro, pico and enterprise small cell base stations. TI's new small cell SoCs are enabled with production ready software and are the highest performing devices available for small cells. Based on TI's innovative KeyStone multicore architecture, these scalable SoCs encompass a mix of processing elements including radio accelerators, network and security coprocessors, combined fixed- and floating-point digital signal processors (DSPs) and an ARM® RISC processor, providing the ideal foundation for layers 1, 2 and 3 and transport processing for high performance small cell base stations.

To view the multimedia assets associated with this release, please click: http://www.prnewswire.com/mnr/texasinstruments/39165/

"Intelligent small cells are the future of public-space mobile data, but their self-organizing capabilities and high traffic environments place huge demands on processing power," said Chris Gilbert, CEO, Ubiquisys. "TI's small cell solution combines dual-mode 3G/LTE flexibility with massive processing power, and harnesses their unparalleled expertise in powering macro networks. We found a true roadmap partner in TI, not just a silicon vendor."

Delivering a comprehensive solution for faster development time

The TCI6612 and TCI6614 SoCs leverage TI's broad resources to bring the most comprehensive portfolio of processing, software and complimentary support devices to small cell developers. The devices are powered by an all-inclusive software suite, based on TI's field-proven wireless application specific libraries, and a full portfolio of complementary analog products such as data converters, RF products, power management, clocks and amplifiers, which complete the integrated solution for small cell developers, reducing system cost and development time. The TCI6612 and TCI6614's processing elements include two or four TMS320C66x fixed- and floating-point DSP cores, as well as a power efficient ARM Cortex™-A8 RISC processor. The ARM core is typically used for control plane processing. The remaining base station functions, including all baseband and packet processing, are handled by the DSP cores coupled with configurable wireless, network and security coprocessors.

"As the mobile market continues to grow, the underlying infrastructure is experiencing greater pressures associated with form factor, performance and power consumption," said Ian Drew, executive vice president of marketing, ARM. "Texas Instruments' use of the ARM Cortex-A8 provides new levels of energy efficiency and higher performance to the small cell base station market."

The TCI6612 and TCI6614 SoCs are code compatible with TI's entire KeyStone multicore portfolio, as well the TMS320C64x DSP generation, ensuring all previous software investments made by TI customers can be reused. This flexibility allows base station manufacturers to develop a wide portfolio of products at a lower cost, lower power, and in less time than with competing solutions.  

Unleashing big performance for small cells

The TCI6612 and TCI6614 SoCs deliver an ideal mix of features for the development of high performance small cell base stations, including:

  • Full LTE and HSPA+ data rate support
  • Programmable capacity for spectrum optimization
  • Enhanced coverage with high data rate mobility

TI's long-standing history and success in the base station market empowers small cell developers to handle large amounts of data traffic with unmatched ease. The TCI6612 and TCI6614 SoCs feature network coprocessors which offload the processing of intensive functions typically performed by DSPs. This frees up MIPs for differentiating features, such as advanced interference cancellation and management techniques, which reduce noise on wireless networks. With TI's new SoCs developers can differentiate their products and come closer than ever before to the boundary of Shannon's Law which defines the limits of wireless data capacity. The result is increased spectral efficiency and higher data rates for operators and a more satisfying user experience. Until today, this kind of performance was beyond the reach of small cell base station manufacturers.

"It's heartening to see that TI doesn't view reaching the limits of Shannon's Law as "fait accompli," said Stephane Teral, principal analyst of mobile and FMC infrastructure, Infonetics Research. "With their new small cell SoCs, TI has shown again the ability of the KeyStone architecture to unleash processing power for the issues operators care about. Spectral efficiency matters as much in small cells as in macro cells. TI just gets it."

Easing operators' migration with dual-mode support

For operators, simultaneous dual-mode support enables parallel execution of two standards supporting deployments such as WCDMA and LTE in a single base station. This allows them to efficiently support 3G to 4G migration and lower CAPEX/OPEX costs by eliminating the need for equipment dedicated to each standard and the need to perform physical upgrades in the field. In addition, the TCI6612 and TCI6614 SoCs are pin and software compatible, offering manufacturers complete flexibility in designing simultaneous dual-mode and multistandard base stations supporting all major 2G, 3G and 4G systems including GSM, CDMA, WCDMA, TD-SCDMA, WiMAX, FDD-LTE and TDD-LTE.

Availability

The TCI6612 and TCI6614 SoCs will begin sampling in 3Q11. Solutions incorporating a digital radio front end will follow. In addition, Azcom Technology currently offers a small cell base station platform to kick-off development.

Visit TI @ Femtocells World Summit

TI is a silver sponsor at the Femtocells World Summit. For customer inquiries, or to view demos in TI's meeting room, please contact Josef Alt ([email protected]) or Sameer Wasson ([email protected]).

TI's KeyStone Multicore Architecture

Texas Instruments' KeyStone multicore architecture is the platform for true multicore innovation, offering developers a robust portfolio of high performance, low-power multicore devices. Unleashing breakthrough performance, the Keystone architecture is the foundation upon which TI's new TMS320C66x DSP generation was developed. KeyStone differs from any other multicore architecture as it has the capacity to provide full processing capability to every core in a multicore device. KeyStone-based devices are optimized for high performance markets including wireless base stations, mission critical, test and automation, medical imaging and high performance computing. Learn more at www.ti.com/c66multicore.

About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks

All trademarks are the property of their respective owners.

SOURCE Texas Instruments Incorporated