TI Home > News Releases

News Releases

TI introduces simple-to-use OpenLink™ Bluetooth® and Wi-Fi® connectivity inside the WiLink™ 6.0 solution for AM18x Sitara™ ARM® Microprocessors

For the first time, Sitara ARM MPU-based devices can leverage pre-integrated, community-backed mac80211 Wi-Fi and BlueZ Bluetooth drivers for cost-effective access point applications

PRNewswire
Jul 11, 2011

DALLAS, July 11, 2011 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NYSE: TXN) today premiered its first module platform housing the WiLink™ 6.0 (WL1271) single-chip, wireless combo solution with TI's open source, Linux-based OpenLink™ drivers. The OpenLink drivers are built on the community-validated mac80211 Wi-Fi driver and BlueZ Bluetooth® protocol stack. The first in a series of such open source platforms from TI, the new WiLink 6.0 OpenLink platform is pre-integrated with TI's AM18x Sitara™ ARM® microprocessors (MPUs). This enables customers developing industrial or point-of-service applications on cost-effective ARM MPUs to easily introduce reliable, low-power Wi-Fi and Bluetooth wireless technologies. More information can be found here:  www.ti.com/am18x-pr

Introducing OpenLink Wi-Fi access points

Today's release also signifies the first time TI's customers can easily repurpose Sitara ARM MPU-based designs as Wi-Fi access points via the new WiLink 6.0 OpenLink platform. OpenLink technology offers mobile-grade, battery-optimized Wi-Fi connectivity supporting native Linux designs, giving customers tested wireless technologies that can be easily re-integrated into designs as they migrate from one kernel version to the next. Additionally, TI's mac80211 Wi-Fi driver is optimized to maximize system level throughput.

As a result, battery-friendly customer products built on Sitara ARM MPUs can serve as a mobile Wi-Fi gateway or support peer-to-peer file transfers with other Wi-Fi enabled devices. These capabilities eliminate the need for external access points and create new opportunities for unique use cases depending on mobile, self-networking devices.

The quick-start experience and other key features

The AM18x Sitara ARM EVM + WL1271 Development Kit is the latest version of TI's original AM18x Sitara ARM EVM and includes elements that create a unique, quick-start experience right out of the box. Meaning a user can be up and running with a demo application in 30 minutes or less.

Other key features include:

Feature

Benefits

OpenLink™ open source drivers
(Wi-Fi and Bluetooth technologies)

  • Native Linux connectivity solutions
  • Simplified re-integration with Linux kernel upgrades
  • Peer-tested technologies

Predefined, validated hardware interfaces and software functionality

  • Minimized risk and design trade-off analysis

WPA supplicant, hostapd, BlueZ Stack, Open Obex software profiles

  • Inclusion of all components required for end-to-end connectivity functionality
  • First-time availability of soft access point via AM18x Sitara ARM EVM

Integrated system components
(all firmware, low-level drivers and applications)

  • Reduced engineering costs, faster time-to-market

Optimized system-level power consumption and throughput

  • Lower power, higher throughput in complex system use cases

Robust TI E2E community and third party support

  • Innovation through collaboration
  • Faster time-to-market

Pricing and availability

The production-ready WiLink 6.0 (WL1271) OpenLink module is packaged as a daughter card and bundled in the AM18x Sitara ARM EVM + WL1271 Development Kit, priced at $1,150.00. For customers already working on an AM18x Sitara ARM EVM, the standalone daughter card is available for $249. [Note: The WiLink 6.0 OpenLink daughter card is compatible with all existing AM18x Sitara ARM EVMs, except the AM1810 Sitara ARM MPU.]


Find out more about TI's wireless connectivity solutions


About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks

WiLink, Sitara and OpenLink are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

www.ti.com/wireless

SOURCE Texas Instruments Incorporated