TI Home > News Releases

News Releases

TI introduces industry's first single-chip battery management device for power tools and e-bike applications

Highly integrated, standalone device provides complete pack protection and cell-balancing for 4- to 10-cell lithium battery packs

PRNewswire
Jul 18, 2011

DALLAS, July 18, 2011 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced the industry's first fully integrated battery protection and cell-balancing solution for Li-Ion and lithium iron phosphate battery packs. The bq77910 battery management and protection device can manage 4- to 10-cell battery packs, and two devices can be stacked to protect 11- to 20-cell packs. The device simplifies battery pack designs for e-bikes, e-scooters, portable gardening tools, power tools and uninterruptible power supplies (UPS) and can also be used when replacing lead acid batteries. For samples and evaluation modules, visit www.ti.com/bq77910-pr.  

(Photo: http://photos.prnewswire.com/prnh/20110718/DA36056)

The bq77910 protects the battery pack by monitoring individual cell voltages and drives two N-channel power MOSFETs to interrupt current flow during fault conditions. Fault detection and recovery criteria for the device are fully programmable in non-volatile memory to suit all types of lithium battery systems.

Key features and benefits of the bq77910

  • Battery management and protection for 4- to 10-cell lithium batteries: Individual cell monitoring and balancing with internal FETs maximizes battery pack service life and performance.
  • Low power operation: Low quiescent current (50 uA typical, 2.5 uA in shutdown mode) minimizes battery discharge during storage or idle periods to optimize battery life.
  • Supports additional lithium battery chemistries: Programmable (EEPROM) fault detection thresholds and time delays make the bq77910 adaptable to all variations of lithium systems, including LiCoO2 and LiFePO4.
  • Standalone integrated solution does not require an external controller or processor.

Tools and support

TI offers a variety of tools and support to speed the implementation of the bq77910 family of devices:


Availability and pricing

The bq77910 is available now in a 38-pin TSSOP package, priced at $2.70 in quantities of 1,000.  

Find out more about TI's battery management portfolio by visiting the links below:


About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks

TI E2E is a trademark of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated