TI Home > News Releases

News Releases

Texas Instruments and UT Austin collaborate to deliver linear algebra library on TI's high performance multicore DSPs

Collaboration enables developers of high performance computing equipment to benefit from lower power systems and more rapid application development

PRNewswire
Nov 16, 2011

SEATTLE, Nov. 14, 2011 /PRNewswire/ -- SUPERCOMPUTING' 2011 -- Setting yet another milestone in multicore innovation, Texas Instruments Incorporated (TI) (NYSE: TXN) and the University of Texas at Austin (UT Austin) have successfully ported UT Austin's libflame library, a dense linear algebra library for scientific computing, to TI's TMS320C6678 multicore digital signal processor (DSP). This port delivers all of libflame's functionalities, providing fundamental software building blocks for many high performance computing (HPC) applications such as oil and gas exploration, financial modeling and molecular dynamics. This achievement demonstrates the fundamental capability of TI's C6678 multicore DSP to implement these algorithms efficiently and also showcases the ease in which such libraries can be ported to TI's DSPs. With an industry-leading 16 GFLOPs/W of single precision performance, TI's C6678 DSP, combined with optimized software libraries like libflame, delivers an ultra-low power solution for the HPC market.

"The speed with which we were able to port a significant scientific computing library like libflame to the C6678 multicore DSP is a testament to the ease of use of TI's DSP and also validates our modern, C-based approach to developing linear algebra libraries," said Robert van de Geijn, professor of computer science, UT Austin, and member of the Texas Institute for Computational Engineering and Sciences.

Earlier today, TI announced it is offering HPC developers the industry's highest performing multicore DSPs at the lowest power levels, based on its TMS320C66x DSP generation. TI's C6678 and TMS320TCI6609 multicore DSPs are ideally suited for computing applications, where ultra- high performance, low power and easy programmability are critical requirements. With the highest performing floating point DSP core at 16 GFLOPs/W, TI's C66x multicore DSPs are changing the way HPC developers meet requirements for applications in oil and gas exploration, financial modeling and molecular dynamics. For more information please visit www.ti.com/multicore.

Visit TI @ SC11

While at SC11, visit TI, in booth #4200 to view the latest multicore solutions and demos for ultra-low power, super high performance computing applications.

For more information:

 

About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story.  Learn more at www.ti.com.

Trademarks

All trademarks are the property of their respective owners.

SOURCE Texas Instruments Incorporated