Dec 22, 2016
DALLAS, Dec. 22, 2016 /PRNewswire/ -- Extending its leadership in the automotive market, Texas Instruments (TI) (NASDAQ: TXN) today announced more than 150 million of its advanced driver assistance systems (ADAS) and digital cockpit Systems-on-Chip (SoCs) are on the road today, in more than 35 OEMs. Leveraging 35 years of automotive experience and billions of analog and embedded processing solutions shipped to automotive manufacturers worldwide, TI created both the TDA and "Jacinto" families of processors to enable designers to deliver applications that are safer and more connected. TI's automotive processors are able to deliver automotive manufacturers what they need to design the next-generation of vehicles that consumers not only want to drive, but with the features they demand. These needs include new applications at an optimized total cost of ownership and with features that are more interactive and responsive than previous vehicles.
Automotive manufacturers benefit from TI's heterogeneous architecture with increased functionality and capability to innovate on the same platform by leveraging installed hardware components and allowing manufacturers to extend current software investment without compromising system performance. This architecture allows for increased concurrencies allowing designers to further extend image, signal and vision processing capabilities. Additionally, TI's automotive processors provide greater power efficiency than other solutions, using general purpose processors and facilitate multi-OS and multi-domain software architecture. Lastly, it offers scalability which maximize investments across multiple models, systems and applications to easily differentiate their offering.
ADAS: a safer driving experience
TI's TDAx driver assistance SoC family offers scalable and open solutions based on a common hardware and software architecture for ADAS applications, including camera-based front (mono/stereo), rear, surround view and night vision systems, and multi-range radar and sensor fusion systems. TI's TDAx SoCs are differentiated by a heterogeneous architecture which integrates purpose-built hardware accelerators (HWA) such as image signal processors (ISPs), embedded vision engines (EVEs) and digital signal processors (DSPs), that are optimized to perform highly complex imaging and signal processing with low power consumption. The members of the TDA family of ADAS processors are:
The award-winning TDA family has also been awarded various awards from Frost & Sullivan industry firm, the Consumers Electronics Show (CES) and Electronic Products magazine.
Digital Cockpit: a more connected driving experience
The "Jacinto" family of processors provides support for a variety of automotive digital cockpit applications including infotainment, head unit co-processing for infotainment, informational ADAS, integrated digital cockpit, digital instrument cluster, head-up display and more. Designed for automotive safety and robustness, "Jacinto" heterogeneous architecture includes hardware firewalls, allows separation between High Level OS (HLOS) and safety OS as well as implementation of robust multi-domain software architecture capable to be ASIL-B safety certified. The processors bring unprecedented feature-rich, in-vehicle infotainment, instrument cluster and telematics features to the next generation of automobiles.
The scalability of the "Jacinto" family allows developers to target specific performance for their applications and leverage headroom using higher performance variants, if required, without software modifications or hardware changes. The "Jacinto 6" family of processors is built on the same architecture, offering software and hardware compatibility with the broadest array of highly scalable ARM® Cortex®-A15 cores for automotive applications. The members of the "Jacinto 6" family of infotainment processors include:
The "Jacinto" family of processors is powering infotainment systems such as Ford SYNC 3®, Volkswagen MIB-II, SAIC-Alibaba "Internet Car" and BMW.
For more information:
Texas Instruments drives automotive innovation
TI's state-of-the-art semiconductor products allow manufacturers and system suppliers to deliver world-class features to the automotive market. Our extensive automotive portfolio includes analog power management, FPD-Link and signal chain solutions, along with DLP® displays, ADAS and infotainment processors, Hercules™ TMS570 safety microcontrollers and wireless connectivity solutions. TI offers SafeTI™ parts designed to facilitate OEMs' compliance with the requirements of ISO 26262, as well as parts specifically designated as compliant with the AEC-Q100 and TS16949 standards, all with excellent product documentation. Visit TI's Automotive page or TI's E2E™ Behind the Wheel Blog to learn more about our commitment to automotive innovation.
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
All trademarks are the property of their respective owners.
SOURCE Texas Instruments