TI Home > News Releases

News Releases

Kick start development of high performance compute systems with TI's new KeyStone™ SoC and evaluation module

Combination of DSP + ARM® cores and high-speed peripherals offer developers an optimal compute solution at low power consumption

Nov 14, 2013

DALLAS, Nov. 14, 2013 /PRNewswire/ -- Further easing the development of processing-intensive applications, Texas Instruments (TI) (NASDAQ: TXN) is unveiling a new system-on-chip (SoC), the 66AK2H14, and evaluation module (EVM) for its KeyStoneTM-based 66AK2Hx family of SoCs. With the new 66AK2H14 device, developers designing high-performance compute systems now have access to a 10Gbps Ethernet switch-on-chip. The inclusion of the 10GigE switch, along with the other high-speed, on-chip interfaces, saves overall board space, reduces chip count and ultimately lowers system cost and power. The EVM enables developers to evaluate and benchmark faster and easier. The 66AK2H14 SoC provides industry-leading computational DSP performance at 307 GMACS/153 GFLOPS and 19600 DMIPS of ARM performance, making it ideal for a wide variety of applications such as video surveillance, radar processing, medical imaging, machine vision and geological exploration.

"Customers today require increased performance to process compute-intensive workloads using less energy in a smaller footprint," said Paul Santeler, vice president and general manager, Hyperscale Business, HP. "As a partner in HP's Moonshot ecosystem dedicated to the rapid development of new Moonshot servers, we believe TI's KeyStone design will provide new capabilities across multiple disciplines to accelerate the pace of telecommunication innovations and geological exploration."

Meet TI's new 10Gbps Ethernet DSP + ARM SoC
TI's newest silicon variant, the 66AK2H14, is the latest addition to its high-performance 66AK2Hx SoC family which integrates multiple ARM Cortex™-A15 MPCore™ processors and TI's fixed- and floating-point TMS320C66x digital signal processor (DSP) generation cores. The 66AK2H14 offers developers exceptional capacity and performance (up to 9.6 GHz of cumulative DSP processing) at industry-leading size, weight, and power. In addition, the new SoC features a wide array of unique high-speed interfaces, including PCIe, RapidIO, Hyperlink, 1Gbps and 10Gbps Ethernet, achieving total I/O throughput of up to 154Gbps. These interfaces are all distinct and not multiplexed, allowing designers tremendous flexibility with uncompromising performance in their designs.

Ease development and debugging with TI's tools and software
TI helps simplify the design process by offering developers highly optimized software for embedded HPC systems along with development and debugging tools for the EVMK2H – all for under $1,000. The EVMK2H features a single 66AK2H14 SoC, a status LCD, two 1Gbps Ethernet RJ-45 interfaces and on-board emulation. An optional EVM breakout card (available separately) also provides two 10Gbps Ethernet optical interfaces for 20Gbps backplane connectivity and optional wire rate switching in high density systems.

The EVMK2H is bundled with TI's Multicore Software Development Kit (MCSDK), enabling faster development with production ready foundational software. The MCSDK eases development and reduces time to market by providing highly-optimized bundles of foundational, platform-specific drivers, optimized libraries and demos.

Complementary analog products to increase system performance
TI offers a wide range of power management and analog signal chain components to increase the system performance of 66AK2H14 SoC-based designs. For example, the TPS53xx integrated FET DC/DC converters provide the highest level of power conversion efficiency even at light loads, while the LM10011 VID converter with dynamic voltage control helps reduce system power consumption. The CDCM6208 low-jitter clock generator also eliminates the need for external buffers, jitter cleaners and level translators.

Availability and pricing
TI's EVMK2H is available now through TI distribution partners or TI.com for $995. In addition to TI's Linux distribution provided in the MCSDK, Wind River® Linux is available now for the 66AK2Hxx family of SoCs. Green Hills® INTEGRITY® RTOS and Wind River VxWorks® RTOS support will each be available before the end of the year. Pricing for the 66AK2H14 SoC will start at $330 for 1 KU. The 10Gbps Ethernet breakout card will be available from Mistral.

Visit TI @ Supercomputing 2013
While at SC13, stop by the TI Booth #3725 to see TI's KeyStone-based HPC systems in action and meet with HPC researchers from TI, industry, and academia.

About TI's KeyStone multicore architecture
TI's KeyStone multicore architecture is the platform for true multicore innovation, offering developers a robust portfolio of high performance, low-power multicore devices. Unleashing breakthrough performance, the KeyStone architecture is the foundation upon which TI's new TMS320C66x DSP generation was developed. KeyStone differs from any other multicore architecture as it has the capacity to provide full processing capability to every core in a multicore device. KeyStone-based devices are optimized for high performance markets including wireless base stations, mission critical, test and automation, medical imaging and high performance computing. Learn more at www.ti.com/multicore.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
All trademarks are the property of their respective owners.

SOURCE Texas Instruments