TI Home > News Releases

News Releases

Achieve improved motion and efficiency for advanced motor control designs in minutes with TI's new InstaSPIN™-MOTION technology

Optimize motor performance across speeds and simplify commissioning, tuning and motion sequencing using C2000™ Piccolo™ microcontrollers.

Apr 18, 2013

HOUSTON, April 18, 2013 /PRNewswire/ -- At long last, system designers have been liberated from limited operating ranges and time-consuming tuning processes with the new InstaSPIN™-MOTION motor control solution from Texas Instruments Incorporated (TI) (NASDAQ: TXN).  InstaSPIN-MOTION is a comprehensive torque-, speed- and motion- control software solution that delivers robust system performance at the highest efficiency for motor applications that operate in various motion state transitions. Built upon TI's InstaSPIN™-FOC motor control solution, InstaSPIN-MOTION is uniquely designed to optimize complex motion sequences, reduce tuning to a single parameter and tracking desired trajectories with unmatched accuracy across operating ranges. It constitutes the easiest and most effective method for achieving optimized sensorless motor control.

TI's InstaSPIN-FOC solution, which was announced earlier this year, takes advantage of the FAST™ premium software sensor for rotor flux measurement and provides motor identification, automatic current control tuning and sensorless feedback in a field-oriented control (FOC) torque controller and speeds deployment of efficient, sensorless, variable load three-phase motor solutions.

InstaSPIN-MOTION further improves motor performance and development time
Adding additional motor control functionality, InstaSPIN-MOTION enables more expertise on chip. With the core algorithms embedded in the read-only-memory (ROM) on TI's 32-bit C2000™ Piccolo™ microcontrollers (MCUs), InstaSPIN-MOTION integrates SpinTAC™ components from LineStream Technologies, featuring optimized motion profiling, single-parameter tuning and a disturbance-rejecting controller, which speeds development and increases performance across changing speeds and loads.  InstaSPIN-MOTION can be used with sensored feedback or with the included sensorless InstaSPIN-FOC solution.

InstaSPIN™-MOTION features and benefits:

  • Eliminate motion control challenges in traditional motor systems. InstaSPIN-MOTION removes the need for inefficient, older design techniques. For example, defining the motor's desired motion in other methods requires simplistic, inflexible trajectories, resulting in mechanical stress. Hand-coded, calculation-heavy trajectories consume valuable memory. Likewise, achieving desired motor performance across varying conditions requires multiple sets of multi-parameter, proportional-integral (PI) controllers needing time-intensive tuning. 
  • InstaSPIN-MOTION's SpinTAC™ components include:
    • IDENTIFY: Ensure optimum tracking and disturbance rejection, working with the real inertia of the system.  
    • CONTROL: Minimize effort and reduce complexity with single coefficient tuning. Rapidly test and tune velocity control from soft to stiff response, defining a controller gain that typically works across the entire variable speed and load range of an application.  Actively estimate and cancel system disturbances in real time, providing maximum performance.
    • MOVE: Produce an automatically optimized motion profile based on start velocity, target velocity and system limitations for acceleration, jerk and motion trajectory type.
    • PLAN: Quickly build various states of motion (speed A to speed B) and tie them together with state-based logic.
  • Develop and evaluate quickly using the new motor control software infrastructure, MotorWare. Take advantage of modules, drivers, system examples and documentation representing the latest in C object-oriented and API-based coding techniques.

Pricing and availability
InstaSPIN-MOTION is available today on the production-ready, 90 MHz, 32-bit floating point Piccolo F2806xM microcontrollers starting at $10.22 USD per 10 Ku.  Designers can begin their latest InstaSPIN-MOTION motor designs with a low-voltage, low-current motor control kit for $299 (DRV8312-69M-KIT), low-voltage, high-current motor control kit for $299 (DRV8301-69M-KIT) or high-voltage motor control kit for $699 (TMDSHVMTRINSPIN). If designers have a previously purchased a TI motor control development kit, they can order the modular InstaSPIN-MOTION-enabled Piccolo controlCARD for $99 (TMDSCNCD28069MISO). If designers purchased any of the above kits with last month's InstaSPIN-FOC announcement, they are already InstaSPIN-MOTION ready, just download the latest kit contents and MotorWare software.

Find out more about InstaSPIN™-MOTION and TI motor control solutions:

TI's broad portfolio of microcontrollers (MCUs) and software
From general purpose, ultra-low power MSP microcontrollers, to Stellaris® Cortex™-M microcontrollers to real-time control C2000™ microcontrollers, and Hercules™ safety microcontrollers, TI offers the broadest range of microcontroller solutions. Designers can accelerate time to market by tapping into TI's complete software and hardware tools, extensive third-party offerings and technical support.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors.  By employing the world's brightest minds, TI creates innovations that shape the future of technology.  TI is helping more than 100,000 customers transform the future, today.  Learn more at www.ti.com.

InstaSPIN, C2000, Piccolo, MSP and MotorWare are trademarks and Stellaris is a registered trademark of Texas Instruments Incorporated. All registered trademarks and other trademarks belong to their respective owners.

SOURCE Texas Instruments