Feb 26, 2013
DALLAS, Feb. 26, 2013 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced the industry's first 35-V, single-channel, output stage power management gate drivers for insulated-gate bipolar transistors (IGBTs) and silicon carbide (SiC) FETs. TI's new UCC27531 and UCC27532 output stage gate drivers with split output provide the most efficient output drive capability, shortest propagation delay and increased system protection for isolated power designs, such as solar DC/AC inverters, uninterruptible power supplies and electric vehicle charging. For more information and samples, visit: www.ti.com/ucc27531-pr.
Today's renewable energy applications require power components that safely deliver more power with greater efficiency. Designers prefer to use IGBTs or the latest SiC FETs that achieve lower power loss at greater than 400 V. Those devices also have standoff voltages up to 1,200 volts, and offer lower ON resistance than equivalent MOSFETs. They are often managed by a TI microcontroller or dedicated digital power controller, such as the UCD3138. Next-generation IGBT- and SiC FET-based designs also require both power and signal isolation from the noisy switching environment of the power stage.
The UCC27531 and UCC27532 prevent the digital controllers from operating too close to the power circuitry, extending the lifetime of isolated power designs.
Key features and benefits of the UCC27531:
Expanding IGBT driver portfolio
The new output stage drivers expand TI's analog and digital controllers that drive IGBTs. Isolated gate drivers, such as the ISO5500, increase safety and system performance in high-current and high-voltage designs. The driver also provides proven reliability of SiO2 dielectric with stability over time, temperature and moisture. TI also has a large portfolio of single and dual 5-A high-speed, low-side power management gate drivers, such as the UCC2751x and UCC2752x families.
Availability and pricing
The UCC27531 and UCC27532 gate drivers are available in a 6-pin, SOT-23 package and are priced at US$0.75 in quantities of 1,000. The UCC27531EVM-184 IGBT driver daughter card evaluation module is priced at US$49 and available for ordering through TI's eStore. In addition, a PSpice model and application note 35-V single-channel gate drivers for IGBTs help speed design time.
Find out more about TI's power management and isolated portfolio:
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
TI E2E, C2000, Delfino and Piccolo are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.
SOURCE Texas Instruments Incorporated