Feb 12, 2013
![]() |
DALLAS, Feb. 12, 2013 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced the industry's smallest off-line, phase-dimmable, constant-current lighting controller and an easy-to-use lighting driver that simplify the retrofit of a variety of LED bulbs, including E14, GU10, A19, PAR20/30/38, MR16 and AR111. The TPS92075 controller and TPS92560 driver reduce component count and solution size while improving compatibility with legacy lighting controls. For more information and samples, visit www.ti.com/tps92560-pr and www.ti.com/tps92075-pr.
The TPS92075 is designed for phase-dimmable, offline AC/DC LED lamp and downlight applications. Offered in a very small 6-pin TSOT package, it achieves power factor correction above 0.9 while delivering smooth, flicker-free dimming when used with conventional wall dimmers. The TPS92560 is intended for use in low-voltage AC or low-voltage DC LED lamp applications such as MR16 and AR111. It uses a proprietary input current control method, which improves compatibility with electronic transformers.
The TPS92075 and TPS92560 join TI's LED driver portfolio for retrofit bulbs that includes the LM3445, LM3447, TPS92310/11/14, LM3444 and LM3401. For more information on LED replacement lamp and downlighting solutions, visit www.ti.com/ledretrofit-pr.
Key features and benefits of TPS92075 and TPS92560:
Availability, packaging and pricing
The TPS92560 and TPS92075 are available in volume now from TI and its authorized distributors. Offered in a 10-pin PowerPad™ MSOP package, the TPS92560 is priced at US$0.72 each in 1,000-unit quantities. Priced at US$0.75, the TPS92075 is offered in an 8-pin SOIC package, and a small 6-pin TSOT package that will be available in March.
Find out more about TI's LED lighting portfolio:
About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.
Trademarks
WEBENCH is a registered trademark and PowerPad, TI E2E and PowerLab are trademarks of Texas Instruments. All other trademarks belong to their respective owners.
SOURCE Texas Instruments Incorporated